![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The build.h file contains the static configuration for the Sensor Fusion based Virtual Orientation sensor adapter. More...
Go to the source code of this file.
Macros | |
| #define | MK64F |
| #define | THISBUILD 420 |
| #define | BOARD_WIN8_REV05 0 |
| #define | BOARD_FRDM_KL25Z 1 |
| #define | BOARD_FRDM_K20D50M 2 |
| #define | BOARD_FRDM_K22F 2 |
| #define | BOARD_FXLC95000CL 3 |
| #define | BOARD_FRDM_KL26Z 4 |
| #define | BOARD_FRDM_K64F 5 |
| #define | BOARD_FRDM_KL16Z 6 |
| #define | BOARD_FRDM_KL46Z 7 |
| #define | BOARD_FRDM_KL46Z_STANDALONE 8 |
| #define | THIS_BOARD_ID BOARD_FRDM_K64F |
The build.h file contains the static configuration for the Sensor Fusion based Virtual Orientation sensor adapter.
Definition in file build.h.
| #define THIS_BOARD_ID BOARD_FRDM_K64F |