![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
fsl_i2c_hal.c implements i2c HAL Layer interfaces. More...
#include "fsl_i2c_hal.h"#include "isf_fsl_i2c_PEx.h"#include "PE_Types.h"#include "isf_i2c_master_adapter.h"#include "fsl_i2c_master_driver.h"
Go to the source code of this file.
Functions | |
| void | i2c_hal_enable (uint32 instance) |
| This function enables the HAL. More... | |
| void | i2c_hal_disable (uint32 instance) |
| This function disables the HAL. More... | |
Variables | |
| i2c_instance_PEx | i2c_instance_tbl [] |
| Lookup table for the LLD instance. More... | |
| i2c_Master_busHandle_t | i2c_master_busHandle [] |
fsl_i2c_hal.c implements i2c HAL Layer interfaces.
File: fsl_i2c_hal.c
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file fsl_i2c_hal.c.
| void i2c_hal_disable | ( | uint32 | instance | ) |
This function disables the HAL.
This allows to perform dynamic OFF the bus.
| [in] | instance | The instance ID/ ID of the bus to disable. |
Definition at line 40 of file fsl_i2c_hal.c.
References i2c_instance_PEx::fnI2CLLDdeviceDis, i2c_Master_BusHandle_struct::master, and I2CMasterState::pDeviceHandle.
Referenced by i2c_master_adapter_stop().

| void i2c_hal_enable | ( | uint32 | instance | ) |
This function enables the HAL.
This allows to perform dynamic ON of the bus.
| [in] | instance | The instance ID/ ID of the bus to enable. |
Definition at line 27 of file fsl_i2c_hal.c.
References i2c_instance_PEx::fnI2CLLDdeviceEn, i2c_Master_BusHandle_struct::master, and I2CMasterState::pDeviceHandle.
Referenced by i2c_master_adapter_start().

| i2c_instance_PEx i2c_instance_tbl[] |
Lookup table for the LLD instance.
Definition at line 25 of file isf_fsl_i2c_PEx.c.
| i2c_Master_busHandle_t i2c_master_busHandle[] |
Definition at line 36 of file isf_sysconf_comms.c.