![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
fsl_i2c_master_driver.h defines structures and types for the i2c master driver. More...
#include <stdlib.h>#include "fsl_i2c_hal.h"#include "PE_Types.h"#include "mqxlite.h"#include "lwevent.h"

Go to the source code of this file.
Data Structures | |
| struct | I2CDeviceInfo |
| Information necessary to communicate with an I2C slave device. More... | |
| struct | sync_object_t |
| Type for an synchronization object. More... | |
| struct | I2CMasterState |
| Internal driver state information. More... | |
Macros | |
| #define | I2C_PEX_WRITE_EVENT_SUCCESS (1) |
| #define | I2C_PEX_WRITE_EVENT_ERROR (I2C_PEX_WRITE_EVENT_SUCCESS << 1) |
| #define | I2C_PEX_READ_EVENT_SUCCESS (I2C_PEX_WRITE_EVENT_ERROR << 1) |
| #define | I2C_PEX_READ_EVENT_ERROR (I2C_PEX_READ_EVENT_SUCCESS << 1) |
Typedefs | |
| typedef struct I2CDeviceInfo | i2c_device_t |
| Information necessary to communicate with an I2C slave device. More... | |
| typedef enum I2CDirection | i2c_direction_t |
| Constants for the direction of an I2C transfer. More... | |
| typedef struct I2CMasterState | i2c_master_t |
| Internal driver state information. More... | |
Enumerations | |
| enum | I2CDirection { kI2CRead = 1, kI2CWrite = 0 } |
| Constants for the direction of an I2C transfer. More... | |
| enum | _i2c_transfer_flags { kI2CNoStart = 1 << 1, kI2CNoStop = 1 << 2 } |
| Optional flags to control a transfer. More... | |
Functions | |
| void | i2c_master_init (uint32_t instance, i2c_master_t *master) |
| Initialize the I2C master mode driver. More... | |
| void | i2c_master_shutdown (i2c_master_t *master) |
| Shut down the driver. More... | |
| i2c_status_t | i2c_master_configure_bus (i2c_master_t *master, const i2c_device_t *device) |
| Configure the I2C bus to access a device. More... | |
| i2c_status_t | i2c_master_transfer (i2c_master_t *master, const i2c_device_t *device, i2c_direction_t direction, bool stopAfterTransfer, uint32_t subaddress, size_t subaddressLength, uint8_t *data, size_t dataLength, size_t *actualLengthTransferred, uint32_t timeout_ms) |
| Perform a blocking read or write transaction on the I2C bus. More... | |
fsl_i2c_master_driver.h defines structures and types for the i2c master driver.
File: fsl_i2c_master_driver.h
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file fsl_i2c_master_driver.h.