|
| void | mma865x_Reset (int32_t *status, void *pSensorHandle) |
| | This function resets the MMA865x sensor resulting in a default configuration for all registers. More...
|
| |
| void | mma865x_CheckId (int32_t *status, void *pSensorHandle) |
| | This function validates the MMA865x sensor is connected via the I2C bus. More...
|
| |
| void | mma865x_SetMode (int32_t *status, void *pSensorHandle, int32_t Mode) |
| | This function sets the MMA865x part to the requested mode. More...
|
| |
| void | mma865x_ValidateConfig (int32_t *status, void *pSensorHandle, void *pSettings) |
| | This function validates the configuration for the MMA865x sensor. More...
|
| |
| isf_dsa_status_t | mma865x_GetConfig (isf_dsa_SensorSettings_t *pRequiredSettings, DeviceDescriptor_t *pDeviceDes) |
| | This function obtains the configuration register values for a given user configuration of the MMA865x. If the configuration has changed then it returns true and saves the new configuration. More...
|
| |
| isf_dsa_status_t | mma865x_SetConfig (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pConfigSettings) |
| | This function sets the MMA865x sensor configuration. More...
|
| |
| isf_dsa_status_t | mma865x_GetData (isf_SensorHandle_t *pSensorHandle, void *pBuffer) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Initialize (isf_SensorHandle_t *pSensorHandle) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_StartData (isf_SensorHandle_t *pSensorHandle) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_EndData (isf_SensorHandle_t *pSensorHandle) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| |
| void | fsl_mma865x_i2c_3D_accel_PeriodicCallback (void *pSensorHandle) |
| |
| isf_dsa_status_t | fsl_mma865x_i2c_3D_accel_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| | This function coverts the raw sample data to the desired output type. More...
|
| |
- Version
- 01.00
Definition in file fsl_mma865x_i2c_3D_accel.c.