![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
fsl_pit_driver.c implements the PIT driver. More...

Go to the source code of this file.
Functions | |
| void | pit_init_module (bool isRunInDebug) |
| Initialize PIT module. More... | |
| void | pit_init_channel (uint32_t timer, const pit_user_config_t *config) |
| Initialize PIT channel. More... | |
| void | pit_shutdown (void) |
| Disable PIT module and gate control. More... | |
| void | pit_timer_start (uint32_t timer) |
| Start timer counting. More... | |
| void | pit_timer_stop (uint32_t timer) |
| Stop timer counting. More... | |
| void | pit_set_timer_period_us (uint32_t timer, uint32_t us) |
| Set timer period in microsecond units. More... | |
| uint32_t | pit_read_timer_us (uint32_t timer) |
| Read current timer value in microsecond units. More... | |
| void | pit_init (bool bEnableirq, uint32 usec) |
| Complete initialization of the PIT timer. More... | |
Variables | |
| uint64_t | pitSourceClock |
fsl_pit_driver.c implements the PIT driver.
File: fsl_pit_driver.c
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file fsl_pit_driver.c.
| uint64_t pitSourceClock |
Definition at line 26 of file fsl_pit_driver.c.
Referenced by pit_init_module(), and pit_read_timer_us().