![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
fsl_uart_common_configurations.c implements UART HAL Layer interfaces. More...
#include "fsl_uart_hal.h"#include "isf_fsl_uart_PEx.h"#include "PE_Types.h"#include "isf_uart_adapter.h"#include "fsl_uart_driver.h"
Go to the source code of this file.
Functions | |
| uart_status_t | uart_hal_init (uint32_t uartInstance, const uart_config_t *config) |
| void | uart_hal_enable_transmitter (uint32_t uartInstance) |
| void | uart_hal_disable_transmitter (uint32_t uartInstance) |
| void | uart_hal_enable_receiver (uint32_t uartInstance) |
| void | uart_hal_disable_receiver (uint32_t uartInstance) |
Variables | |
| uint8 | gSys_NumUARTBuses |
fsl_uart_common_configurations.c implements UART HAL Layer interfaces.
File: fsl_uart_common_configurations.c
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file fsl_uart_common_configurations.c.
| void uart_hal_disable_receiver | ( | uint32_t | uartInstance | ) |
Definition at line 81 of file fsl_uart_common_configurations.c.
References gSys_NumUARTBuses.
| void uart_hal_disable_transmitter | ( | uint32_t | uartInstance | ) |
Definition at line 52 of file fsl_uart_common_configurations.c.
References gSys_NumUARTBuses.
| void uart_hal_enable_receiver | ( | uint32_t | uartInstance | ) |
Definition at line 68 of file fsl_uart_common_configurations.c.
References gSys_NumUARTBuses.
| void uart_hal_enable_transmitter | ( | uint32_t | uartInstance | ) |
Definition at line 40 of file fsl_uart_common_configurations.c.
References gSys_NumUARTBuses.
| uart_status_t uart_hal_init | ( | uint32_t | uartInstance, |
| const uart_config_t * | config | ||
| ) |
Definition at line 27 of file fsl_uart_common_configurations.c.
References gSys_NumUARTBuses, kStatus_UART_Error, and kStatus_UART_Success.
| uint8 gSys_NumUARTBuses |
Definition at line 63 of file isf_sysconf_comms.c.
Referenced by uart_hal_disable_receiver(), uart_hal_disable_transmitter(), uart_hal_enable_receiver(), uart_hal_enable_transmitter(), and uart_hal_init().