![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
fsl_uart_driver.h defines structures and types for the i2c master driver. More...
#include <stdint.h>#include <stdbool.h>#include "PE_Types.h"#include "mqxlite.h"#include "lwevent.h"#include "fsl_uart_hal.h"

Go to the source code of this file.
Data Structures | |
| struct | UartState |
| Runtime state of the UART driver. More... | |
| struct | UartUserConfig |
| User configuration structure for UART driver. More... | |
Macros | |
| #define | UART_PEX_WRITE_EVENT_SUCCESS (1) |
| #define | UART_PEX_WRITE_EVENT_ERROR (UART_PEX_WRITE_EVENT_SUCCESS << 1) |
| #define | UART_PEX_READ_EVENT_SUCCESS (UART_PEX_WRITE_EVENT_ERROR << 1) |
| #define | UART_PEX_READ_EVENT_ERROR (UART_PEX_READ_EVENT_SUCCESS << 1) |
Typedefs | |
| typedef struct UartState | uart_state_t |
| Runtime state of the UART driver. More... | |
| typedef struct UartUserConfig | uart_user_config_t |
| User configuration structure for UART driver. More... | |
Functions | |
| uart_status_t | uart_init (uint32_t uartInstance, uart_state_t *uartState, const uart_user_config_t *uartUserConfig) |
| This function initializes a UART instance for operation. More... | |
| uart_status_t | uart_send_data (uart_state_t *uartState, const uint8_t *sendBuffer, uint32_t txByteCount, uint32_t timeout) |
| This function sends (transmits) data out through the UART module using a blocking method. More... | |
| uart_status_t | uart_send_data_async (uart_state_t *uartState, const uint8_t *sendBuffer, uint32_t txByteCount) |
| This function sends (transmits) data through the UART module using a non-blocking method. More... | |
| uart_status_t | uart_get_transmit_status (uart_state_t *uartState, uint32_t *bytesTransmitted) |
| This function returns whether the previous UART transmit has finished. More... | |
| uart_status_t | uart_get_receive_status (uart_state_t *uartState, uint32_t *bytesReceived) |
| This function returns whether the previous UART receive is complete. More... | |
| uart_status_t | uart_receive_data (uart_state_t *uartState, uint8_t *rxBuffer, uint32_t requestedByteCount, uint32_t timeout) |
| This function gets (receives) data from the UART module using a blocking method. More... | |
| uart_status_t | uart_receive_data_async (uart_state_t *uartState, uint8_t *rxBuffer, uint32_t requestedByteCount) |
| This function gets (receives) data from the UART module using a non-blocking method. More... | |
fsl_uart_driver.h defines structures and types for the i2c master driver.
File: fsl_uart_driver.h
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file fsl_uart_driver.h.