![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The fusion_config.h file contains additional static configuration for the Sensor Fusion based Virtual Orientation sensor adapter. More...
#include "fusion_types.h"

Go to the source code of this file.
The fusion_config.h file contains additional static configuration for the Sensor Fusion based Virtual Orientation sensor adapter.
Definition in file fusion_config.h.
| #define ACCEL_GET_HAL_X_VALUE | ( | v | ) | (v) |
Definition at line 45 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define ACCEL_GET_HAL_Y_VALUE | ( | v | ) | (v) |
Definition at line 47 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define ACCEL_GET_HAL_Z_VALUE | ( | v | ) | (v) |
Definition at line 49 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define ACCEL_HAL_X_INDEX Y |
Definition at line 46 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define ACCEL_HAL_Y_INDEX X |
Definition at line 48 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define ACCEL_HAL_Z_INDEX Z |
Definition at line 50 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define ACCEL_OVERSAMPLE_RATIO 4 |
Definition at line 22 of file fusion_config.h.
Referenced by fRun_3DOF_G_BASIC().
| #define ALGO_CHOICE Q9 |
Definition at line 26 of file fusion_config.h.
| #define COMPUTE_3DOF_B_BASIC |
Definition at line 30 of file fusion_config.h.
| #define COMPUTE_3DOF_G_BASIC |
Definition at line 29 of file fusion_config.h.
| #define COMPUTE_3DOF_Y_BASIC |
Definition at line 31 of file fusion_config.h.
| #define COMPUTE_6DOF_GB_BASIC |
Definition at line 32 of file fusion_config.h.
| #define COMPUTE_6DOF_GY_KALMAN |
Definition at line 33 of file fusion_config.h.
| #define COMPUTE_9DOF_GBY_KALMAN |
Definition at line 34 of file fusion_config.h.
| #define GYRO_GET_HAL_X_VALUE | ( | v | ) | (-(v)) |
Definition at line 57 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define GYRO_GET_HAL_Y_VALUE | ( | v | ) | (-(v)) |
Definition at line 59 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define GYRO_GET_HAL_Z_VALUE | ( | v | ) | (-(v)) |
Definition at line 61 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define GYRO_HAL_X_INDEX Y |
Definition at line 58 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define GYRO_HAL_Y_INDEX X |
Definition at line 60 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define GYRO_HAL_Z_INDEX Z |
Definition at line 62 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define GYRO_OVERSAMPLE_RATIO 16 |
Definition at line 24 of file fusion_config.h.
Referenced by fRun_1DOF_P_BASIC(), fRun_3DOF_Y_BASIC(), fRun_6DOF_GB_BASIC(), fRun_6DOF_GY_KALMAN(), fRun_9DOF_GBY_KALMAN(), and Fusion_Run().
| #define MAG_GET_HAL_X_VALUE | ( | v | ) | (-(v)) |
Definition at line 51 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define MAG_GET_HAL_Y_VALUE | ( | v | ) | (-(v)) |
Definition at line 53 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define MAG_GET_HAL_Z_VALUE | ( | v | ) | (v) |
Definition at line 55 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define MAG_HAL_X_INDEX Y |
Definition at line 52 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define MAG_HAL_Y_INDEX X |
Definition at line 54 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define MAG_HAL_Z_INDEX Z |
Definition at line 56 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().
| #define MAG_OVERSAMPLE_RATIO 4 |
Definition at line 23 of file fusion_config.h.
Referenced by fRun_3DOF_B_BASIC(), and fRunMagCalibration().
| #define ORIENTATION_OUTPUT_PERIOD_USECS 40000 |
Definition at line 20 of file fusion_config.h.
| #define PARALLELNOTSEQUENTIAL 1 |
Definition at line 17 of file fusion_config.h.
Referenced by Fusion_Run().
| #define PRESSURE_OVERSAMPLE_RATIO 1 |
Definition at line 25 of file fusion_config.h.
| #define SENSORFS (uint32)(1000000.0F/((float)ORIENTATION_OUTPUT_PERIOD_USECS)) |
Definition at line 21 of file fusion_config.h.
Referenced by fRun_1DOF_P_BASIC(), fRun_3DOF_B_BASIC(), fRun_3DOF_G_BASIC(), fRun_3DOF_Y_BASIC(), fRun_6DOF_GB_BASIC(), fRun_6DOF_GY_KALMAN(), fRun_9DOF_GBY_KALMAN(), and fRunMagCalibration().
| #define THISCOORDSYSTEM NED |
Definition at line 37 of file fusion_config.h.
Referenced by fRun_9DOF_GBY_KALMAN(), and Fusion_Run().
| #define USE_ACCELEROMETER |
Definition at line 39 of file fusion_config.h.
| #define USE_GYROMETER |
Definition at line 41 of file fusion_config.h.
| #define USE_MAGNETOMETER |
Definition at line 40 of file fusion_config.h.
Referenced by fsl_fusion_virt_3D_orient_Shutdown().