![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | BMTimer1_TDeviceData |
Macros | |
| #define | AVAILABLE_EVENTS_MASK (LDD_TEventMask)(LDD_TIMERUNIT_ON_COUNTER_RESTART) |
| #define | __BWUserType_BMTimer1_TValueType |
| #define | BMTimer1_CNT_INP_FREQ_U_0 0x016E3600UL /* Counter input frequency in Hz */ |
| #define | BMTimer1_CNT_INP_FREQ_R_0 23999808.00153599F /* Counter input frequency in Hz */ |
| #define | BMTimer1_CNT_INP_FREQ_COUNT 0U /* Count of predefined counter input frequencies */ |
| #define | BMTimer1_PERIOD_TICKS 0x016E3600UL /* Initialization value of period in 'counter ticks' */ |
| #define | BMTimer1_NUMBER_OF_CHANNELS 0x00U /* Count of predefined channels */ |
| #define | BMTimer1_COUNTER_WIDTH 0x20U /* Counter width in bits */ |
| #define | BMTimer1_COUNTER_DIR DIR_DOWN /* Direction of counting */ |
| #define | BMTimer1_PRPH_BASE_ADDRESS 0x40037000U |
| #define | BMTimer1_Init_METHOD_ENABLED |
| #define | BMTimer1_Deinit_METHOD_ENABLED |
| #define | BMTimer1_Enable_METHOD_ENABLED |
| #define | BMTimer1_Disable_METHOD_ENABLED |
| #define | BMTimer1_SetPeriodTicks_METHOD_ENABLED |
| #define | BMTimer1_GetPeriodTicks_METHOD_ENABLED |
| #define | BMTimer1_ResetCounter_METHOD_ENABLED |
| #define | BMTimer1_GetCounterValue_METHOD_ENABLED |
| #define | BMTimer1_OnCounterRestart_EVENT_ENABLED |
Typedefs | |
| typedef BMTimer1_TDeviceData * | BMTimer1_TDeviceDataPtr |
| typedef uint32_t | BMTimer1_TValueType |
Functions | |
| LDD_TDeviceData * | BMTimer1_Init (LDD_TUserData *UserDataPtr) |
| Initializes the device. Allocates memory for the device data structure, allocates interrupt vectors and sets interrupt priority, sets pin routing, sets timing, etc. If the property ["Enable in init. code"] is set to "yes" value then the device is also enabled (see the description of the [Enable] method). In this case the [Enable] method is not necessary and needn't to be generated. This method can be called only once. Before the second call of Init the [Deinit] must be called first. More... | |
| void | BMTimer1_Deinit (LDD_TDeviceData *DeviceDataPtr) |
| Deinitializes the device. Switches off the device, frees the device data structure memory, interrupts vectors, etc. More... | |
| LDD_TError | BMTimer1_Enable (LDD_TDeviceData *DeviceDataPtr) |
| Enables the component - it starts the signal generation. Events may be generated (see SetEventMask). The method is not available if the counter can't be disabled/enabled by HW. More... | |
| LDD_TError | BMTimer1_Disable (LDD_TDeviceData *DeviceDataPtr) |
| Disables the component - it stops signal generation and events calling. The method is not available if the counter can't be disabled/enabled by HW. More... | |
| LDD_TError | BMTimer1_SetPeriodTicks (LDD_TDeviceData *DeviceDataPtr, BMTimer1_TValueType Ticks) |
| The method sets timer re-initialization period (in timer ticks). This method is available only if the property ["Counter restart"] is switched to 'on-match' value. More... | |
| LDD_TError | BMTimer1_GetPeriodTicks (LDD_TDeviceData *DeviceDataPtr, BMTimer1_TValueType *TicksPtr) |
| Returns the number of counter ticks before re-initialization. See also method [SetPeriodTicks]. This method is available only if the property ["Counter restart"] is switched to 'on-match' value. More... | |
| LDD_TError | BMTimer1_ResetCounter (LDD_TDeviceData *DeviceDataPtr) |
| Resets counter. If counter is counting up then it is set to zero. If counter is counting down then counter is updated to the reload value. The method is not available if HW doesn't allow resetting of the counter. More... | |
| BMTimer1_TValueType | BMTimer1_GetCounterValue (LDD_TDeviceData *DeviceDataPtr) |
| Returns the content of counter register. This method can be used both if counter is enabled and if counter is disabled. The method is not available if HW doesn't allow reading of the counter. More... | |
| void | BMTimer1_Interrupt (LDD_RTOS_TISRParameter _isrParameter) |
| #define __BWUserType_BMTimer1_TValueType |
Definition at line 125 of file BMTimer1.h.
| #define AVAILABLE_EVENTS_MASK (LDD_TEventMask)(LDD_TIMERUNIT_ON_COUNTER_RESTART) |
Definition at line 128 of file BMTimer1.c.
| #define BMTimer1_CNT_INP_FREQ_COUNT 0U /* Count of predefined counter input frequencies */ |
Definition at line 130 of file BMTimer1.h.
| #define BMTimer1_CNT_INP_FREQ_R_0 23999808.00153599F /* Counter input frequency in Hz */ |
Definition at line 129 of file BMTimer1.h.
| #define BMTimer1_CNT_INP_FREQ_U_0 0x016E3600UL /* Counter input frequency in Hz */ |
Definition at line 128 of file BMTimer1.h.
| #define BMTimer1_COUNTER_DIR DIR_DOWN /* Direction of counting */ |
Definition at line 134 of file BMTimer1.h.
| #define BMTimer1_COUNTER_WIDTH 0x20U /* Counter width in bits */ |
Definition at line 133 of file BMTimer1.h.
| #define BMTimer1_Deinit_METHOD_ENABLED |
Deinit method of the component BMTimer1 is enabled (generated)
Definition at line 140 of file BMTimer1.h.
| #define BMTimer1_Disable_METHOD_ENABLED |
Disable method of the component BMTimer1 is enabled (generated)
Definition at line 142 of file BMTimer1.h.
| #define BMTimer1_Enable_METHOD_ENABLED |
Enable method of the component BMTimer1 is enabled (generated)
Definition at line 141 of file BMTimer1.h.
| #define BMTimer1_GetCounterValue_METHOD_ENABLED |
GetCounterValue method of the component BMTimer1 is enabled (generated)
Definition at line 146 of file BMTimer1.h.
| #define BMTimer1_GetPeriodTicks_METHOD_ENABLED |
GetPeriodTicks method of the component BMTimer1 is enabled (generated)
Definition at line 144 of file BMTimer1.h.
| #define BMTimer1_Init_METHOD_ENABLED |
Init method of the component BMTimer1 is enabled (generated)
Definition at line 139 of file BMTimer1.h.
| #define BMTimer1_NUMBER_OF_CHANNELS 0x00U /* Count of predefined channels */ |
Definition at line 132 of file BMTimer1.h.
| #define BMTimer1_OnCounterRestart_EVENT_ENABLED |
OnCounterRestart event of the component BMTimer1 is enabled (generated)
Definition at line 149 of file BMTimer1.h.
| #define BMTimer1_PERIOD_TICKS 0x016E3600UL /* Initialization value of period in 'counter ticks' */ |
Definition at line 131 of file BMTimer1.h.
| #define BMTimer1_PRPH_BASE_ADDRESS 0x40037000U |
Peripheral base address of a device allocated by the component. This constant can be used directly in PDD macros.
Definition at line 136 of file BMTimer1.h.
| #define BMTimer1_ResetCounter_METHOD_ENABLED |
ResetCounter method of the component BMTimer1 is enabled (generated)
Definition at line 145 of file BMTimer1.h.
| #define BMTimer1_SetPeriodTicks_METHOD_ENABLED |
SetPeriodTicks method of the component BMTimer1 is enabled (generated)
Definition at line 143 of file BMTimer1.h.
Definition at line 123 of file BMTimer1.c.
| typedef uint32_t BMTimer1_TValueType |
Definition at line 126 of file BMTimer1.h.
| void BMTimer1_Deinit | ( | LDD_TDeviceData * | DeviceDataPtr | ) |
Deinitializes the device. Switches off the device, frees the device data structure memory, interrupts vectors, etc.
| DeviceDataPtr | - Device data structure pointer returned by Init method |
Definition at line 201 of file BMTimer1.c.
| LDD_TError BMTimer1_Disable | ( | LDD_TDeviceData * | DeviceDataPtr | ) |
Disables the component - it stops signal generation and events calling. The method is not available if the counter can't be disabled/enabled by HW.
| DeviceDataPtr | - Device data structure pointer returned by [Init] method. |
Definition at line 263 of file BMTimer1.c.
| LDD_TError BMTimer1_Enable | ( | LDD_TDeviceData * | DeviceDataPtr | ) |
Enables the component - it starts the signal generation. Events may be generated (see SetEventMask). The method is not available if the counter can't be disabled/enabled by HW.
| DeviceDataPtr | - Device data structure pointer returned by [Init] method. |
Definition at line 237 of file BMTimer1.c.
| BMTimer1_TValueType BMTimer1_GetCounterValue | ( | LDD_TDeviceData * | DeviceDataPtr | ) |
Returns the content of counter register. This method can be used both if counter is enabled and if counter is disabled. The method is not available if HW doesn't allow reading of the counter.
| DeviceDataPtr | - Device data structure pointer returned by [Init] method. |
Definition at line 387 of file BMTimer1.c.
| LDD_TError BMTimer1_GetPeriodTicks | ( | LDD_TDeviceData * | DeviceDataPtr, |
| BMTimer1_TValueType * | TicksPtr | ||
| ) |
Returns the number of counter ticks before re-initialization. See also method [SetPeriodTicks]. This method is available only if the property ["Counter restart"] is switched to 'on-match' value.
| DeviceDataPtr | - Device data structure pointer returned by [Init] method. |
| TicksPtr | - Pointer to return value of the number of counter ticks before re-initialization |
Definition at line 328 of file BMTimer1.c.
| LDD_TDeviceData * BMTimer1_Init | ( | LDD_TUserData * | UserDataPtr | ) |
Initializes the device. Allocates memory for the device data structure, allocates interrupt vectors and sets interrupt priority, sets pin routing, sets timing, etc. If the property ["Enable in init. code"] is set to "yes" value then the device is also enabled (see the description of the [Enable] method). In this case the [Enable] method is not necessary and needn't to be generated. This method can be called only once. Before the second call of Init the [Deinit] must be called first.
| UserDataPtr | - Pointer to the user or RTOS specific data. This pointer will be passed as an event or callback parameter. |
Definition at line 155 of file BMTimer1.c.
References BMTimer1_Interrupt(), BMTimer1_TDeviceData::SavedISRSettings_TUInterrupt, and BMTimer1_TDeviceData::UserDataPtr.

| void BMTimer1_Interrupt | ( | LDD_RTOS_TISRParameter | _isrParameter | ) |
Definition at line 403 of file BMTimer1.c.
References BMTimer1_OnCounterRestart(), and BMTimer1_TDeviceData::UserDataPtr.
Referenced by BMTimer1_Init().


| LDD_TError BMTimer1_ResetCounter | ( | LDD_TDeviceData * | DeviceDataPtr | ) |
Resets counter. If counter is counting up then it is set to zero. If counter is counting down then counter is updated to the reload value. The method is not available if HW doesn't allow resetting of the counter.
| DeviceDataPtr | - Device data structure pointer returned by [Init] method. |
Definition at line 356 of file BMTimer1.c.
| LDD_TError BMTimer1_SetPeriodTicks | ( | LDD_TDeviceData * | DeviceDataPtr, |
| BMTimer1_TValueType | Ticks | ||
| ) |
The method sets timer re-initialization period (in timer ticks). This method is available only if the property ["Counter restart"] is switched to 'on-match' value.
| DeviceDataPtr | - Device data structure pointer returned by [Init] method. |
| Ticks | - Number of counter ticks before counter re-initialization. Value 0 means maximal period value the same as "free-running mode", e.g. counter overflow or underflow without any explicit re-initialization. |
Definition at line 297 of file BMTimer1.c.