![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | FXAS21002_1_DATA_TYPE fxas21002_DataBuffer_t |
Variables | |
| fxas21002_Sensor_Specific_Settings_t | FXAS21002_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXAS21002_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXAS21002_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| fxas21002_Sensor_Specific_Settings_t | FXAS21002_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | FXAS21002_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | FXAS21002_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define FXAS21002_1_DATA_TYPE fxas21002_DataBuffer_t |
Definition at line 54 of file FXAS21002_1.h.
| const isf_dsa_Adapter_t FXAS21002_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 54 of file FXAS21002_1.c.
| const isf_dsa_Adapter_t FXAS21002_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 54 of file FXAS21002_1.c.
| const i2c_device_t FXAS21002_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 69 of file FXAS21002_1.c.
| const i2c_device_t FXAS21002_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 69 of file FXAS21002_1.c.
| fxas21002_Sensor_Specific_Settings_t FXAS21002_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 36 of file FXAS21002_1.c.
| fxas21002_Sensor_Specific_Settings_t FXAS21002_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 36 of file FXAS21002_1.c.