![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | MAG3110_1_DATA_TYPE mag3110_DataBuffer_t |
Variables | |
| mag3110_Sensor_Specific_Settings_t | MAG3110_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MAG3110_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MAG3110_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| mag3110_Sensor_Specific_Settings_t | MAG3110_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MAG3110_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MAG3110_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define MAG3110_1_DATA_TYPE mag3110_DataBuffer_t |
Definition at line 55 of file MAG3110_1.h.
| const isf_dsa_Adapter_t MAG3110_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 59 of file MAG3110_1.c.
| const isf_dsa_Adapter_t MAG3110_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 59 of file MAG3110_1.c.
| const i2c_device_t MAG3110_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 74 of file MAG3110_1.c.
| const i2c_device_t MAG3110_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 74 of file MAG3110_1.c.
| mag3110_Sensor_Specific_Settings_t MAG3110_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 38 of file MAG3110_1.c.
| mag3110_Sensor_Specific_Settings_t MAG3110_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 38 of file MAG3110_1.c.