![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | MMA865x_1_DATA_TYPE mma865x_DataBuffer_t |
Variables | |
| mma865x_Sensor_Specific_Settings_t | MMA865x_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MMA865x_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MMA865x_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| mma865x_Sensor_Specific_Settings_t | MMA865x_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MMA865x_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MMA865x_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
| #define MMA865x_1_DATA_TYPE mma865x_DataBuffer_t |
Definition at line 55 of file MMA865x_1.h.
| const isf_dsa_Adapter_t MMA865x_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 79 of file MMA865x_1.c.
| const isf_dsa_Adapter_t MMA865x_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 79 of file MMA865x_1.c.
| const i2c_device_t MMA865x_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 94 of file MMA865x_1.c.
| const i2c_device_t MMA865x_1_DeviceInfo |
This allows access to the sensor communications specific configuration.
Definition at line 94 of file MMA865x_1.c.
| mma865x_Sensor_Specific_Settings_t MMA865x_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 38 of file MMA865x_1.c.
| mma865x_Sensor_Specific_Settings_t MMA865x_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 38 of file MMA865x_1.c.