![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | ORIENT_1_DATA_TYPE fsl_orientation_DataBuffer_t |
Functions | |
| void | Fusion_Task_task (uint32_t task_init_data) |
| void | MagCal_Task_task (uint32_t task_init_data) |
Variables | |
| fsl_fusion_Sensor_Specific_Settings_t | ORIENT_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | ORIENT_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| fsl_fusion_Sensor_Specific_Settings_t | ORIENT_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | ORIENT_1_Adapter |
| This allows access to the sensor adapter instance for the target sensor. More... | |
| #define ORIENT_1_DATA_TYPE fsl_orientation_DataBuffer_t |
Definition at line 52 of file ORIENT_1.h.
| void Fusion_Task_task | ( | uint32_t | task_init_data | ) |
Definition at line 83 of file ORIENT_1.c.
References fsl_fusion_task().

| void MagCal_Task_task | ( | uint32_t | task_init_data | ) |
Definition at line 98 of file ORIENT_1.c.
References fsl_MagCal_task().

| const isf_dsa_Adapter_t ORIENT_1_Adapter |
This creates the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 61 of file ORIENT_1.c.
| const isf_dsa_Adapter_t ORIENT_1_Adapter |
This allows access to the sensor adapter instance for the target sensor.
This allows access to the sensor adapter instance for the target sensor.
Definition at line 61 of file ORIENT_1.c.
| fsl_fusion_Sensor_Specific_Settings_t ORIENT_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 39 of file ORIENT_1.c.
| fsl_fusion_Sensor_Specific_Settings_t ORIENT_1_Sensor_Specific_Config |
This allows access to the sensor specific configuration for the target sensor.
Definition at line 39 of file ORIENT_1.c.