![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Macros | |
| #define | PEX_VECTOR_TABLE 0x01U /* Vector table is managed by PEx */ |
| #define | VECTOR_SP_MAIN &__SP_INIT /* 0x00 - ivINT_Initial_Stack_Pointer used by PE */ |
| #define | VECTOR_1 (tIsrFunc)&__boot /* 0x01 - ivINT_Initial_Program_Counter used by PE */ |
| #define | VECTOR_2 (tIsrFunc)&UnhandledInterrupt /* 0x02 -2 ivINT_NMI unused by PE */ |
| #define | VECTOR_3 (tIsrFunc)&UnhandledInterrupt /* 0x03 -1 ivINT_Hard_Fault unused by PE */ |
| #define | VECTOR_4 (tIsrFunc)&UnhandledInterrupt /* 0x04 - ivINT_Mem_Manage_Fault unused by PE */ |
| #define | VECTOR_5 (tIsrFunc)&UnhandledInterrupt /* 0x05 - ivINT_Bus_Fault unused by PE */ |
| #define | VECTOR_6 (tIsrFunc)&UnhandledInterrupt /* 0x06 - ivINT_Usage_Fault unused by PE */ |
| #define | VECTOR_7 (tIsrFunc)&UnhandledInterrupt /* 0x07 - ivINT_Reserved7 unused by PE */ |
| #define | VECTOR_8 (tIsrFunc)&UnhandledInterrupt /* 0x08 - ivINT_Reserved8 unused by PE */ |
| #define | VECTOR_9 (tIsrFunc)&UnhandledInterrupt /* 0x09 - ivINT_Reserved9 unused by PE */ |
| #define | VECTOR_10 (tIsrFunc)&UnhandledInterrupt /* 0x0A - ivINT_Reserved10 unused by PE */ |
| #define | VECTOR_11 (tIsrFunc)&_svc_handler /* 0x0B - ivINT_SVCall used by PE */ |
| #define | VECTOR_12 (tIsrFunc)&UnhandledInterrupt /* 0x0C - ivINT_DebugMonitor unused by PE */ |
| #define | VECTOR_13 (tIsrFunc)&UnhandledInterrupt /* 0x0D - ivINT_Reserved13 unused by PE */ |
| #define | VECTOR_14 (tIsrFunc)&_pend_svc /* 0x0E - ivINT_PendableSrvReq used by PE */ |
| #define | VECTOR_15 (tIsrFunc)&_int_kernel_isr /* 0x0F 112 ivINT_SysTick used by PE */ |
| #define | VECTOR_16 (tIsrFunc)&_int_kernel_isr /* 0x10 - ivINT_DMA0 used by PE */ |
| #define | VECTOR_17 (tIsrFunc)&_int_kernel_isr /* 0x11 - ivINT_DMA1 used by PE */ |
| #define | VECTOR_18 (tIsrFunc)&_int_kernel_isr /* 0x12 - ivINT_DMA2 used by PE */ |
| #define | VECTOR_19 (tIsrFunc)&_int_kernel_isr /* 0x13 - ivINT_DMA3 used by PE */ |
| #define | VECTOR_20 (tIsrFunc)&_int_kernel_isr /* 0x14 - ivINT_DMA4 used by PE */ |
| #define | VECTOR_21 (tIsrFunc)&_int_kernel_isr /* 0x15 - ivINT_DMA5 used by PE */ |
| #define | VECTOR_22 (tIsrFunc)&_int_kernel_isr /* 0x16 - ivINT_DMA6 used by PE */ |
| #define | VECTOR_23 (tIsrFunc)&_int_kernel_isr /* 0x17 - ivINT_DMA7 used by PE */ |
| #define | VECTOR_24 (tIsrFunc)&_int_kernel_isr /* 0x18 - ivINT_DMA8 used by PE */ |
| #define | VECTOR_25 (tIsrFunc)&_int_kernel_isr /* 0x19 - ivINT_DMA9 used by PE */ |
| #define | VECTOR_26 (tIsrFunc)&_int_kernel_isr /* 0x1A - ivINT_DMA10 used by PE */ |
| #define | VECTOR_27 (tIsrFunc)&_int_kernel_isr /* 0x1B - ivINT_DMA11 used by PE */ |
| #define | VECTOR_28 (tIsrFunc)&_int_kernel_isr /* 0x1C - ivINT_DMA12 used by PE */ |
| #define | VECTOR_29 (tIsrFunc)&_int_kernel_isr /* 0x1D - ivINT_DMA13 used by PE */ |
| #define | VECTOR_30 (tIsrFunc)&_int_kernel_isr /* 0x1E - ivINT_DMA14 used by PE */ |
| #define | VECTOR_31 (tIsrFunc)&_int_kernel_isr /* 0x1F - ivINT_DMA15 used by PE */ |
| #define | VECTOR_32 (tIsrFunc)&_int_kernel_isr /* 0x20 - ivINT_DMA_Error used by PE */ |
| #define | VECTOR_33 (tIsrFunc)&_int_kernel_isr /* 0x21 - ivINT_MCM used by PE */ |
| #define | VECTOR_34 (tIsrFunc)&_int_kernel_isr /* 0x22 - ivINT_FTFE used by PE */ |
| #define | VECTOR_35 (tIsrFunc)&_int_kernel_isr /* 0x23 - ivINT_Read_Collision used by PE */ |
| #define | VECTOR_36 (tIsrFunc)&_int_kernel_isr /* 0x24 - ivINT_LVD_LVW used by PE */ |
| #define | VECTOR_37 (tIsrFunc)&_int_kernel_isr /* 0x25 - ivINT_LLW used by PE */ |
| #define | VECTOR_38 (tIsrFunc)&_int_kernel_isr /* 0x26 - ivINT_Watchdog used by PE */ |
| #define | VECTOR_39 (tIsrFunc)&_int_kernel_isr /* 0x27 - ivINT_RNG used by PE */ |
| #define | VECTOR_40 (tIsrFunc)&_int_kernel_isr /* 0x28 - ivINT_I2C0 used by PE */ |
| #define | VECTOR_41 (tIsrFunc)&_int_kernel_isr /* 0x29 112 ivINT_I2C1 used by PE */ |
| #define | VECTOR_42 (tIsrFunc)&_int_kernel_isr /* 0x2A 112 ivINT_SPI0 used by PE */ |
| #define | VECTOR_43 (tIsrFunc)&_int_kernel_isr /* 0x2B - ivINT_SPI1 used by PE */ |
| #define | VECTOR_44 (tIsrFunc)&_int_kernel_isr /* 0x2C - ivINT_I2S0_Tx used by PE */ |
| #define | VECTOR_45 (tIsrFunc)&_int_kernel_isr /* 0x2D - ivINT_I2S0_Rx used by PE */ |
| #define | VECTOR_46 (tIsrFunc)&_int_kernel_isr /* 0x2E - ivINT_UART0_LON used by PE */ |
| #define | VECTOR_47 (tIsrFunc)&_int_kernel_isr /* 0x2F 112 ivINT_UART0_RX_TX used by PE */ |
| #define | VECTOR_48 (tIsrFunc)&_int_kernel_isr /* 0x30 112 ivINT_UART0_ERR used by PE */ |
| #define | VECTOR_49 (tIsrFunc)&_int_kernel_isr /* 0x31 - ivINT_UART1_RX_TX used by PE */ |
| #define | VECTOR_50 (tIsrFunc)&_int_kernel_isr /* 0x32 - ivINT_UART1_ERR used by PE */ |
| #define | VECTOR_51 (tIsrFunc)&_int_kernel_isr /* 0x33 - ivINT_UART2_RX_TX used by PE */ |
| #define | VECTOR_52 (tIsrFunc)&_int_kernel_isr /* 0x34 - ivINT_UART2_ERR used by PE */ |
| #define | VECTOR_53 (tIsrFunc)&_int_kernel_isr /* 0x35 - ivINT_UART3_RX_TX used by PE */ |
| #define | VECTOR_54 (tIsrFunc)&_int_kernel_isr /* 0x36 - ivINT_UART3_ERR used by PE */ |
| #define | VECTOR_55 (tIsrFunc)&_int_kernel_isr /* 0x37 - ivINT_ADC0 used by PE */ |
| #define | VECTOR_56 (tIsrFunc)&_int_kernel_isr /* 0x38 - ivINT_CMP0 used by PE */ |
| #define | VECTOR_57 (tIsrFunc)&_int_kernel_isr /* 0x39 - ivINT_CMP1 used by PE */ |
| #define | VECTOR_58 (tIsrFunc)&_int_kernel_isr /* 0x3A - ivINT_FTM0 used by PE */ |
| #define | VECTOR_59 (tIsrFunc)&_int_kernel_isr /* 0x3B - ivINT_FTM1 used by PE */ |
| #define | VECTOR_60 (tIsrFunc)&_int_kernel_isr /* 0x3C - ivINT_FTM2 used by PE */ |
| #define | VECTOR_61 (tIsrFunc)&_int_kernel_isr /* 0x3D - ivINT_CMT used by PE */ |
| #define | VECTOR_62 (tIsrFunc)&_int_kernel_isr /* 0x3E - ivINT_RTC used by PE */ |
| #define | VECTOR_63 (tIsrFunc)&_int_kernel_isr /* 0x3F - ivINT_RTC_Seconds used by PE */ |
| #define | VECTOR_64 (tIsrFunc)&_int_kernel_isr /* 0x40 112 ivINT_PIT0 used by PE */ |
| #define | VECTOR_65 (tIsrFunc)&_int_kernel_isr /* 0x41 - ivINT_PIT1 used by PE */ |
| #define | VECTOR_66 (tIsrFunc)&_int_kernel_isr /* 0x42 - ivINT_PIT2 used by PE */ |
| #define | VECTOR_67 (tIsrFunc)&_int_kernel_isr /* 0x43 - ivINT_PIT3 used by PE */ |
| #define | VECTOR_68 (tIsrFunc)&_int_kernel_isr /* 0x44 - ivINT_PDB0 used by PE */ |
| #define | VECTOR_69 (tIsrFunc)&_int_kernel_isr /* 0x45 - ivINT_USB0 used by PE */ |
| #define | VECTOR_70 (tIsrFunc)&_int_kernel_isr /* 0x46 - ivINT_USBDCD used by PE */ |
| #define | VECTOR_71 (tIsrFunc)&_int_kernel_isr /* 0x47 - ivINT_Reserved71 used by PE */ |
| #define | VECTOR_72 (tIsrFunc)&_int_kernel_isr /* 0x48 - ivINT_DAC0 used by PE */ |
| #define | VECTOR_73 (tIsrFunc)&_int_kernel_isr /* 0x49 - ivINT_MCG used by PE */ |
| #define | VECTOR_74 (tIsrFunc)&_int_kernel_isr /* 0x4A - ivINT_LPTimer used by PE */ |
| #define | VECTOR_75 (tIsrFunc)&_int_kernel_isr /* 0x4B - ivINT_PORTA used by PE */ |
| #define | VECTOR_76 (tIsrFunc)&_int_kernel_isr /* 0x4C - ivINT_PORTB used by PE */ |
| #define | VECTOR_77 (tIsrFunc)&_int_kernel_isr /* 0x4D - ivINT_PORTC used by PE */ |
| #define | VECTOR_78 (tIsrFunc)&_int_kernel_isr /* 0x4E - ivINT_PORTD used by PE */ |
| #define | VECTOR_79 (tIsrFunc)&_int_kernel_isr /* 0x4F - ivINT_PORTE used by PE */ |
| #define | VECTOR_80 (tIsrFunc)&_int_kernel_isr /* 0x50 - ivINT_SWI used by PE */ |
| #define | VECTOR_81 (tIsrFunc)&_int_kernel_isr /* 0x51 - ivINT_SPI2 used by PE */ |
| #define | VECTOR_82 (tIsrFunc)&_int_kernel_isr /* 0x52 - ivINT_UART4_RX_TX used by PE */ |
| #define | VECTOR_83 (tIsrFunc)&_int_kernel_isr /* 0x53 - ivINT_UART4_ERR used by PE */ |
| #define | VECTOR_84 (tIsrFunc)&_int_kernel_isr /* 0x54 - ivINT_UART5_RX_TX used by PE */ |
| #define | VECTOR_85 (tIsrFunc)&_int_kernel_isr /* 0x55 - ivINT_UART5_ERR used by PE */ |
| #define | VECTOR_86 (tIsrFunc)&_int_kernel_isr /* 0x56 - ivINT_CMP2 used by PE */ |
| #define | VECTOR_87 (tIsrFunc)&_int_kernel_isr /* 0x57 - ivINT_FTM3 used by PE */ |
| #define | VECTOR_88 (tIsrFunc)&_int_kernel_isr /* 0x58 - ivINT_Reserved88 used by PE */ |
| #define | VECTOR_89 (tIsrFunc)&_int_kernel_isr /* 0x59 - ivINT_ADC1 used by PE */ |
| #define | VECTOR_90 (tIsrFunc)&_int_kernel_isr /* 0x5A - ivINT_I2C2 used by PE */ |
| #define | VECTOR_91 (tIsrFunc)&_int_kernel_isr /* 0x5B - ivINT_CAN0_ORed_Message_buffer used by PE */ |
| #define | VECTOR_92 (tIsrFunc)&_int_kernel_isr /* 0x5C - ivINT_CAN0_Bus_Off used by PE */ |
| #define | VECTOR_93 (tIsrFunc)&_int_kernel_isr /* 0x5D - ivINT_CAN0_Error used by PE */ |
| #define | VECTOR_94 (tIsrFunc)&_int_kernel_isr /* 0x5E - ivINT_CAN0_Tx_Warning used by PE */ |
| #define | VECTOR_95 (tIsrFunc)&_int_kernel_isr /* 0x5F - ivINT_CAN0_Rx_Warning used by PE */ |
| #define | VECTOR_96 (tIsrFunc)&_int_kernel_isr /* 0x60 - ivINT_CAN0_Wake_Up used by PE */ |
| #define | VECTOR_97 (tIsrFunc)&_int_kernel_isr /* 0x61 - ivINT_SDHC used by PE */ |
| #define | VECTOR_98 (tIsrFunc)&_int_kernel_isr /* 0x62 - ivINT_ENET_1588_Timer used by PE */ |
| #define | VECTOR_99 (tIsrFunc)&_int_kernel_isr /* 0x63 - ivINT_ENET_Transmit used by PE */ |
| #define | VECTOR_100 (tIsrFunc)&_int_kernel_isr /* 0x64 - ivINT_ENET_Receive used by PE */ |
| #define | VECTOR_101 (tIsrFunc)&_int_kernel_isr /* 0x65 - ivINT_ENET_Error used by PE */ |
| #define PEX_VECTOR_TABLE 0x01U /* Vector table is managed by PEx */ |
Definition at line 84 of file Vectors_Config.h.
| #define VECTOR_1 (tIsrFunc)&__boot /* 0x01 - ivINT_Initial_Program_Counter used by PE */ |
Definition at line 88 of file Vectors_Config.h.
| #define VECTOR_10 (tIsrFunc)&UnhandledInterrupt /* 0x0A - ivINT_Reserved10 unused by PE */ |
Definition at line 97 of file Vectors_Config.h.
| #define VECTOR_100 (tIsrFunc)&_int_kernel_isr /* 0x64 - ivINT_ENET_Receive used by PE */ |
Definition at line 187 of file Vectors_Config.h.
| #define VECTOR_101 (tIsrFunc)&_int_kernel_isr /* 0x65 - ivINT_ENET_Error used by PE */ |
Definition at line 188 of file Vectors_Config.h.
| #define VECTOR_11 (tIsrFunc)&_svc_handler /* 0x0B - ivINT_SVCall used by PE */ |
Definition at line 98 of file Vectors_Config.h.
| #define VECTOR_12 (tIsrFunc)&UnhandledInterrupt /* 0x0C - ivINT_DebugMonitor unused by PE */ |
Definition at line 99 of file Vectors_Config.h.
| #define VECTOR_13 (tIsrFunc)&UnhandledInterrupt /* 0x0D - ivINT_Reserved13 unused by PE */ |
Definition at line 100 of file Vectors_Config.h.
| #define VECTOR_14 (tIsrFunc)&_pend_svc /* 0x0E - ivINT_PendableSrvReq used by PE */ |
Definition at line 101 of file Vectors_Config.h.
| #define VECTOR_15 (tIsrFunc)&_int_kernel_isr /* 0x0F 112 ivINT_SysTick used by PE */ |
Definition at line 102 of file Vectors_Config.h.
| #define VECTOR_16 (tIsrFunc)&_int_kernel_isr /* 0x10 - ivINT_DMA0 used by PE */ |
Definition at line 103 of file Vectors_Config.h.
| #define VECTOR_17 (tIsrFunc)&_int_kernel_isr /* 0x11 - ivINT_DMA1 used by PE */ |
Definition at line 104 of file Vectors_Config.h.
| #define VECTOR_18 (tIsrFunc)&_int_kernel_isr /* 0x12 - ivINT_DMA2 used by PE */ |
Definition at line 105 of file Vectors_Config.h.
| #define VECTOR_19 (tIsrFunc)&_int_kernel_isr /* 0x13 - ivINT_DMA3 used by PE */ |
Definition at line 106 of file Vectors_Config.h.
| #define VECTOR_2 (tIsrFunc)&UnhandledInterrupt /* 0x02 -2 ivINT_NMI unused by PE */ |
Definition at line 89 of file Vectors_Config.h.
| #define VECTOR_20 (tIsrFunc)&_int_kernel_isr /* 0x14 - ivINT_DMA4 used by PE */ |
Definition at line 107 of file Vectors_Config.h.
| #define VECTOR_21 (tIsrFunc)&_int_kernel_isr /* 0x15 - ivINT_DMA5 used by PE */ |
Definition at line 108 of file Vectors_Config.h.
| #define VECTOR_22 (tIsrFunc)&_int_kernel_isr /* 0x16 - ivINT_DMA6 used by PE */ |
Definition at line 109 of file Vectors_Config.h.
| #define VECTOR_23 (tIsrFunc)&_int_kernel_isr /* 0x17 - ivINT_DMA7 used by PE */ |
Definition at line 110 of file Vectors_Config.h.
| #define VECTOR_24 (tIsrFunc)&_int_kernel_isr /* 0x18 - ivINT_DMA8 used by PE */ |
Definition at line 111 of file Vectors_Config.h.
| #define VECTOR_25 (tIsrFunc)&_int_kernel_isr /* 0x19 - ivINT_DMA9 used by PE */ |
Definition at line 112 of file Vectors_Config.h.
| #define VECTOR_26 (tIsrFunc)&_int_kernel_isr /* 0x1A - ivINT_DMA10 used by PE */ |
Definition at line 113 of file Vectors_Config.h.
| #define VECTOR_27 (tIsrFunc)&_int_kernel_isr /* 0x1B - ivINT_DMA11 used by PE */ |
Definition at line 114 of file Vectors_Config.h.
| #define VECTOR_28 (tIsrFunc)&_int_kernel_isr /* 0x1C - ivINT_DMA12 used by PE */ |
Definition at line 115 of file Vectors_Config.h.
| #define VECTOR_29 (tIsrFunc)&_int_kernel_isr /* 0x1D - ivINT_DMA13 used by PE */ |
Definition at line 116 of file Vectors_Config.h.
| #define VECTOR_3 (tIsrFunc)&UnhandledInterrupt /* 0x03 -1 ivINT_Hard_Fault unused by PE */ |
Definition at line 90 of file Vectors_Config.h.
| #define VECTOR_30 (tIsrFunc)&_int_kernel_isr /* 0x1E - ivINT_DMA14 used by PE */ |
Definition at line 117 of file Vectors_Config.h.
| #define VECTOR_31 (tIsrFunc)&_int_kernel_isr /* 0x1F - ivINT_DMA15 used by PE */ |
Definition at line 118 of file Vectors_Config.h.
| #define VECTOR_32 (tIsrFunc)&_int_kernel_isr /* 0x20 - ivINT_DMA_Error used by PE */ |
Definition at line 119 of file Vectors_Config.h.
| #define VECTOR_33 (tIsrFunc)&_int_kernel_isr /* 0x21 - ivINT_MCM used by PE */ |
Definition at line 120 of file Vectors_Config.h.
| #define VECTOR_34 (tIsrFunc)&_int_kernel_isr /* 0x22 - ivINT_FTFE used by PE */ |
Definition at line 121 of file Vectors_Config.h.
| #define VECTOR_35 (tIsrFunc)&_int_kernel_isr /* 0x23 - ivINT_Read_Collision used by PE */ |
Definition at line 122 of file Vectors_Config.h.
| #define VECTOR_36 (tIsrFunc)&_int_kernel_isr /* 0x24 - ivINT_LVD_LVW used by PE */ |
Definition at line 123 of file Vectors_Config.h.
| #define VECTOR_37 (tIsrFunc)&_int_kernel_isr /* 0x25 - ivINT_LLW used by PE */ |
Definition at line 124 of file Vectors_Config.h.
| #define VECTOR_38 (tIsrFunc)&_int_kernel_isr /* 0x26 - ivINT_Watchdog used by PE */ |
Definition at line 125 of file Vectors_Config.h.
| #define VECTOR_39 (tIsrFunc)&_int_kernel_isr /* 0x27 - ivINT_RNG used by PE */ |
Definition at line 126 of file Vectors_Config.h.
| #define VECTOR_4 (tIsrFunc)&UnhandledInterrupt /* 0x04 - ivINT_Mem_Manage_Fault unused by PE */ |
Definition at line 91 of file Vectors_Config.h.
| #define VECTOR_40 (tIsrFunc)&_int_kernel_isr /* 0x28 - ivINT_I2C0 used by PE */ |
Definition at line 127 of file Vectors_Config.h.
| #define VECTOR_41 (tIsrFunc)&_int_kernel_isr /* 0x29 112 ivINT_I2C1 used by PE */ |
Definition at line 128 of file Vectors_Config.h.
| #define VECTOR_42 (tIsrFunc)&_int_kernel_isr /* 0x2A 112 ivINT_SPI0 used by PE */ |
Definition at line 129 of file Vectors_Config.h.
| #define VECTOR_43 (tIsrFunc)&_int_kernel_isr /* 0x2B - ivINT_SPI1 used by PE */ |
Definition at line 130 of file Vectors_Config.h.
| #define VECTOR_44 (tIsrFunc)&_int_kernel_isr /* 0x2C - ivINT_I2S0_Tx used by PE */ |
Definition at line 131 of file Vectors_Config.h.
| #define VECTOR_45 (tIsrFunc)&_int_kernel_isr /* 0x2D - ivINT_I2S0_Rx used by PE */ |
Definition at line 132 of file Vectors_Config.h.
| #define VECTOR_46 (tIsrFunc)&_int_kernel_isr /* 0x2E - ivINT_UART0_LON used by PE */ |
Definition at line 133 of file Vectors_Config.h.
| #define VECTOR_47 (tIsrFunc)&_int_kernel_isr /* 0x2F 112 ivINT_UART0_RX_TX used by PE */ |
Definition at line 134 of file Vectors_Config.h.
| #define VECTOR_48 (tIsrFunc)&_int_kernel_isr /* 0x30 112 ivINT_UART0_ERR used by PE */ |
Definition at line 135 of file Vectors_Config.h.
| #define VECTOR_49 (tIsrFunc)&_int_kernel_isr /* 0x31 - ivINT_UART1_RX_TX used by PE */ |
Definition at line 136 of file Vectors_Config.h.
| #define VECTOR_5 (tIsrFunc)&UnhandledInterrupt /* 0x05 - ivINT_Bus_Fault unused by PE */ |
Definition at line 92 of file Vectors_Config.h.
| #define VECTOR_50 (tIsrFunc)&_int_kernel_isr /* 0x32 - ivINT_UART1_ERR used by PE */ |
Definition at line 137 of file Vectors_Config.h.
| #define VECTOR_51 (tIsrFunc)&_int_kernel_isr /* 0x33 - ivINT_UART2_RX_TX used by PE */ |
Definition at line 138 of file Vectors_Config.h.
| #define VECTOR_52 (tIsrFunc)&_int_kernel_isr /* 0x34 - ivINT_UART2_ERR used by PE */ |
Definition at line 139 of file Vectors_Config.h.
| #define VECTOR_53 (tIsrFunc)&_int_kernel_isr /* 0x35 - ivINT_UART3_RX_TX used by PE */ |
Definition at line 140 of file Vectors_Config.h.
| #define VECTOR_54 (tIsrFunc)&_int_kernel_isr /* 0x36 - ivINT_UART3_ERR used by PE */ |
Definition at line 141 of file Vectors_Config.h.
| #define VECTOR_55 (tIsrFunc)&_int_kernel_isr /* 0x37 - ivINT_ADC0 used by PE */ |
Definition at line 142 of file Vectors_Config.h.
| #define VECTOR_56 (tIsrFunc)&_int_kernel_isr /* 0x38 - ivINT_CMP0 used by PE */ |
Definition at line 143 of file Vectors_Config.h.
| #define VECTOR_57 (tIsrFunc)&_int_kernel_isr /* 0x39 - ivINT_CMP1 used by PE */ |
Definition at line 144 of file Vectors_Config.h.
| #define VECTOR_58 (tIsrFunc)&_int_kernel_isr /* 0x3A - ivINT_FTM0 used by PE */ |
Definition at line 145 of file Vectors_Config.h.
| #define VECTOR_59 (tIsrFunc)&_int_kernel_isr /* 0x3B - ivINT_FTM1 used by PE */ |
Definition at line 146 of file Vectors_Config.h.
| #define VECTOR_6 (tIsrFunc)&UnhandledInterrupt /* 0x06 - ivINT_Usage_Fault unused by PE */ |
Definition at line 93 of file Vectors_Config.h.
| #define VECTOR_60 (tIsrFunc)&_int_kernel_isr /* 0x3C - ivINT_FTM2 used by PE */ |
Definition at line 147 of file Vectors_Config.h.
| #define VECTOR_61 (tIsrFunc)&_int_kernel_isr /* 0x3D - ivINT_CMT used by PE */ |
Definition at line 148 of file Vectors_Config.h.
| #define VECTOR_62 (tIsrFunc)&_int_kernel_isr /* 0x3E - ivINT_RTC used by PE */ |
Definition at line 149 of file Vectors_Config.h.
| #define VECTOR_63 (tIsrFunc)&_int_kernel_isr /* 0x3F - ivINT_RTC_Seconds used by PE */ |
Definition at line 150 of file Vectors_Config.h.
| #define VECTOR_64 (tIsrFunc)&_int_kernel_isr /* 0x40 112 ivINT_PIT0 used by PE */ |
Definition at line 151 of file Vectors_Config.h.
| #define VECTOR_65 (tIsrFunc)&_int_kernel_isr /* 0x41 - ivINT_PIT1 used by PE */ |
Definition at line 152 of file Vectors_Config.h.
| #define VECTOR_66 (tIsrFunc)&_int_kernel_isr /* 0x42 - ivINT_PIT2 used by PE */ |
Definition at line 153 of file Vectors_Config.h.
| #define VECTOR_67 (tIsrFunc)&_int_kernel_isr /* 0x43 - ivINT_PIT3 used by PE */ |
Definition at line 154 of file Vectors_Config.h.
| #define VECTOR_68 (tIsrFunc)&_int_kernel_isr /* 0x44 - ivINT_PDB0 used by PE */ |
Definition at line 155 of file Vectors_Config.h.
| #define VECTOR_69 (tIsrFunc)&_int_kernel_isr /* 0x45 - ivINT_USB0 used by PE */ |
Definition at line 156 of file Vectors_Config.h.
| #define VECTOR_7 (tIsrFunc)&UnhandledInterrupt /* 0x07 - ivINT_Reserved7 unused by PE */ |
Definition at line 94 of file Vectors_Config.h.
| #define VECTOR_70 (tIsrFunc)&_int_kernel_isr /* 0x46 - ivINT_USBDCD used by PE */ |
Definition at line 157 of file Vectors_Config.h.
| #define VECTOR_71 (tIsrFunc)&_int_kernel_isr /* 0x47 - ivINT_Reserved71 used by PE */ |
Definition at line 158 of file Vectors_Config.h.
| #define VECTOR_72 (tIsrFunc)&_int_kernel_isr /* 0x48 - ivINT_DAC0 used by PE */ |
Definition at line 159 of file Vectors_Config.h.
| #define VECTOR_73 (tIsrFunc)&_int_kernel_isr /* 0x49 - ivINT_MCG used by PE */ |
Definition at line 160 of file Vectors_Config.h.
| #define VECTOR_74 (tIsrFunc)&_int_kernel_isr /* 0x4A - ivINT_LPTimer used by PE */ |
Definition at line 161 of file Vectors_Config.h.
| #define VECTOR_75 (tIsrFunc)&_int_kernel_isr /* 0x4B - ivINT_PORTA used by PE */ |
Definition at line 162 of file Vectors_Config.h.
| #define VECTOR_76 (tIsrFunc)&_int_kernel_isr /* 0x4C - ivINT_PORTB used by PE */ |
Definition at line 163 of file Vectors_Config.h.
| #define VECTOR_77 (tIsrFunc)&_int_kernel_isr /* 0x4D - ivINT_PORTC used by PE */ |
Definition at line 164 of file Vectors_Config.h.
| #define VECTOR_78 (tIsrFunc)&_int_kernel_isr /* 0x4E - ivINT_PORTD used by PE */ |
Definition at line 165 of file Vectors_Config.h.
| #define VECTOR_79 (tIsrFunc)&_int_kernel_isr /* 0x4F - ivINT_PORTE used by PE */ |
Definition at line 166 of file Vectors_Config.h.
| #define VECTOR_8 (tIsrFunc)&UnhandledInterrupt /* 0x08 - ivINT_Reserved8 unused by PE */ |
Definition at line 95 of file Vectors_Config.h.
| #define VECTOR_80 (tIsrFunc)&_int_kernel_isr /* 0x50 - ivINT_SWI used by PE */ |
Definition at line 167 of file Vectors_Config.h.
| #define VECTOR_81 (tIsrFunc)&_int_kernel_isr /* 0x51 - ivINT_SPI2 used by PE */ |
Definition at line 168 of file Vectors_Config.h.
| #define VECTOR_82 (tIsrFunc)&_int_kernel_isr /* 0x52 - ivINT_UART4_RX_TX used by PE */ |
Definition at line 169 of file Vectors_Config.h.
| #define VECTOR_83 (tIsrFunc)&_int_kernel_isr /* 0x53 - ivINT_UART4_ERR used by PE */ |
Definition at line 170 of file Vectors_Config.h.
| #define VECTOR_84 (tIsrFunc)&_int_kernel_isr /* 0x54 - ivINT_UART5_RX_TX used by PE */ |
Definition at line 171 of file Vectors_Config.h.
| #define VECTOR_85 (tIsrFunc)&_int_kernel_isr /* 0x55 - ivINT_UART5_ERR used by PE */ |
Definition at line 172 of file Vectors_Config.h.
| #define VECTOR_86 (tIsrFunc)&_int_kernel_isr /* 0x56 - ivINT_CMP2 used by PE */ |
Definition at line 173 of file Vectors_Config.h.
| #define VECTOR_87 (tIsrFunc)&_int_kernel_isr /* 0x57 - ivINT_FTM3 used by PE */ |
Definition at line 174 of file Vectors_Config.h.
| #define VECTOR_88 (tIsrFunc)&_int_kernel_isr /* 0x58 - ivINT_Reserved88 used by PE */ |
Definition at line 175 of file Vectors_Config.h.
| #define VECTOR_89 (tIsrFunc)&_int_kernel_isr /* 0x59 - ivINT_ADC1 used by PE */ |
Definition at line 176 of file Vectors_Config.h.
| #define VECTOR_9 (tIsrFunc)&UnhandledInterrupt /* 0x09 - ivINT_Reserved9 unused by PE */ |
Definition at line 96 of file Vectors_Config.h.
| #define VECTOR_90 (tIsrFunc)&_int_kernel_isr /* 0x5A - ivINT_I2C2 used by PE */ |
Definition at line 177 of file Vectors_Config.h.
| #define VECTOR_91 (tIsrFunc)&_int_kernel_isr /* 0x5B - ivINT_CAN0_ORed_Message_buffer used by PE */ |
Definition at line 178 of file Vectors_Config.h.
| #define VECTOR_92 (tIsrFunc)&_int_kernel_isr /* 0x5C - ivINT_CAN0_Bus_Off used by PE */ |
Definition at line 179 of file Vectors_Config.h.
| #define VECTOR_93 (tIsrFunc)&_int_kernel_isr /* 0x5D - ivINT_CAN0_Error used by PE */ |
Definition at line 180 of file Vectors_Config.h.
| #define VECTOR_94 (tIsrFunc)&_int_kernel_isr /* 0x5E - ivINT_CAN0_Tx_Warning used by PE */ |
Definition at line 181 of file Vectors_Config.h.
| #define VECTOR_95 (tIsrFunc)&_int_kernel_isr /* 0x5F - ivINT_CAN0_Rx_Warning used by PE */ |
Definition at line 182 of file Vectors_Config.h.
| #define VECTOR_96 (tIsrFunc)&_int_kernel_isr /* 0x60 - ivINT_CAN0_Wake_Up used by PE */ |
Definition at line 183 of file Vectors_Config.h.
| #define VECTOR_97 (tIsrFunc)&_int_kernel_isr /* 0x61 - ivINT_SDHC used by PE */ |
Definition at line 184 of file Vectors_Config.h.
| #define VECTOR_98 (tIsrFunc)&_int_kernel_isr /* 0x62 - ivINT_ENET_1588_Timer used by PE */ |
Definition at line 185 of file Vectors_Config.h.
| #define VECTOR_99 (tIsrFunc)&_int_kernel_isr /* 0x63 - ivINT_ENET_Transmit used by PE */ |
Definition at line 186 of file Vectors_Config.h.
| #define VECTOR_SP_MAIN &__SP_INIT /* 0x00 - ivINT_Initial_Stack_Pointer used by PE */ |
Definition at line 87 of file Vectors_Config.h.