![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | dataPair_t |
| struct | fLfiTable_t |
| struct | mpl3115_Specific_Settings_t |
| This structure defines important settings. More... | |
| struct | mpl3115_DataBuffer_t |
| This structure defines the dummy DSA data buffer format. More... | |
Macros | |
| #define | MPL3115_PRESS_FLOAT_CONVERSION_FACTOR 0.000000061035 |
| #define | MPL3115_PRESS_FLOAT_CONVERSION_OFFSET 0.0 |
| #define | MPL3115_PRESS_FIXED_CONVERSION_FACTOR (1000/4) |
| #define | MPL3115_PRESS_FIXED_CONVERSION_OFFSET 0 |
| #define | MPL3115_ALT_FLOAT_CONVERSION_FACTOR 1.0 |
| #define | MPL3115_ALT_FLOAT_CONVERSION_OFFSET 0.0 |
| #define | MPL3115_ALT_FIXED_CONVERSION_FACTOR 1 |
| #define | MPL3115_ALT_FIXED_CONVERSION_OFFSET 0 |
| #define | MPL3115_TEMP_FLOAT_CONVERSION_FACTOR 256.0 |
| #define | MPL3115_TEMP_FLOAT_CONVERSION_OFFSET 0.0 |
| #define | MPL3115_TEMP_FIXED_CONVERSION_FACTOR 256 |
| #define | MPL3115_TEMP_FIXED_CONVERSION_OFFSET 0 |
| #define | MPL3115_ONE_SECOND 1000000 |
| #define | BYTES_FOR_FULL_READ 5 |
| This function retrieves the raw data from the MPL3115 sensor. More... | |
| #define | MPL3115_DEBUG 0 |
| #define | ABSOLUTE_VALUE(x) ( (x) < 0.0 ? (-(x)) : (x)) |
| #define | ZERO_EPSILON (1.0E-10) |
| #define | IS_PRACTICALLY_ZERO(x) ( ABSOLUTE_VALUE(x) < ZERO_EPSILON ) |
Enumerations | |
| enum | { LFI_NO_EXTRAPOLATION = 0, LFI_TABLE_LIMITS = 1, LFI_EXTRAPOLATE = 2 } |
| enum | { LFI_SUCCESS = 0, LFI_BAD_TABLE = -1, LFI_BAD_PTR = -2, LFI_OUT_OF_RANGE = -3 } |
| enum | { FSL_MPL3115_ACCEL_800HZ = 1250, FSL_MPL3115_ACCEL_400HZ = 2500, FSL_MPL3115_ACCEL_200HZ = 5000, FSL_MPL3115_ACCEL_100HZ = 10000, FSL_MPL3115_ACCEL_50HZ = 20000, FSL_MPL3115_ACCEL_12p5HZ = 80000, FSL_MPL3115_ACCEL_6p25HZ = 160000, FSL_MPL3115_ACCEL_1p56HZ = 640000 } |
| This enumerator describes the available sample rates for the MPL3115 accelerometer. More... | |
| enum | { FSL_MPL3115_ACCEL_SCALE_2G = 0, FSL_MPL3115_ACCEL_SCALE_4G = 1, FSL_MPL3115_ACCEL_SCALE_8G = 2 } |
| This enumerator describes the available acceleration ranges for the MM865X family of accelerometers. More... | |
Functions | |
| long | fLfi (const fLfiTable_t *lookupTable, float lFiIn, float *lfiOut) |
| void | mpl3115_Reset (int32_t *status, void *pSensorHandle) |
| This function resets the MPL3115 sensor resulting in a default configuration for all registers. More... | |
| void | mpl3115_CheckId (int32_t *status, void *pSensorHandle) |
| This function validates the MPL3115 sensor is connected via the I2C bus. More... | |
| void | mpl3115_SetMode (int32_t *status, void *pSensorHandle, int32_t Mode) |
| This function sets the MPL3115 part to the requested mode. More... | |
| void | mpl3115_ValidateConfig (int32_t *status, void *pSensorHandle, void *pSettings) |
| This function validates the configuration for the MPL3115 sensor. More... | |
| isf_dsa_status_t | mpl3115_SetConfig (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pConfigSettings) |
| This function sets the MPL3115 sensor configuration. More... | |
| int32 | convertPressureToAltitude (uint32 pressure) |
| isf_dsa_status_t | mpl3115_GetData (isf_SensorHandle_t *pSensorHandle, mpl3115_DataBuffer_t *pData) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_Initialize (isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_ValidateSettings (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_Configure (isf_SensorHandle_t *pSensorHandle, isf_dsa_SensorSettings_t *pSensorSettings) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_StartData (isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_EndData (isf_SensorHandle_t *pSensorHandle) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_Calibrate (isf_SensorHandle_t *pSensorHandle, void *pCalData) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_Shutdown (isf_SensorHandle_t *pSensorHandle) |
| void | fsl_mpl3115_i2c_1D_press_PeriodicCallback (void *pSensorHandle) |
| isf_dsa_status_t | fsl_mpl3115_i2c_1D_press_Convert (volatile isf_SensorHandle_t *pSensorHandle, isf_SensorDataTypes_t convertToType, isf_dsa_result_types_t resultType, void *pNativeSample, void *pConvertedSample, int32 *numBytes) |
| This function coverts the raw sample data to the desired output type. More... | |
| void | mpl3115_ReadRegisters (isf_SensorHandle_t *pSensorHandle) |
Variables | |
| isf_SensorTypes_t | mpl3115_SupportedSensorTypes [] = { TYPE_THERMOMETER, TYPE_ALTIMETER, TYPE_BAROMETER, TYPE_ABSOLUTE_PRESSURE_SENSOR, TYPE_NATIVE_SENSOR_TYPE } |
| Supported sensor and data types for MPL3115. More... | |
| isf_SensorDataTypes_t | mpl3115_SupportedDataTypes [] = { TYPE_TEMPERATURE, TYPE_ALTITUDE, TYPE_PRESSURE, TYPE_NATIVE_SENSOR_DATA_TYPE } |
| isf_SensorTypes_t | mpl3115_SupportedSensorTypes [] |
| Supported sensor and data types for MPL3115. More... | |
| isf_SensorDataTypes_t | mpl3115_SupportedDataTypes [] |
| #define ABSOLUTE_VALUE | ( | x | ) | ( (x) < 0.0 ? (-(x)) : (x)) |
Definition at line 994 of file fsl_mpl3115_i2c_1D_press.c.
| #define BYTES_FOR_FULL_READ 5 |
This function retrieves the raw data from the MPL3115 sensor.
Definition at line 902 of file fsl_mpl3115_i2c_1D_press.c.
Referenced by mpl3115_GetData().
| #define IS_PRACTICALLY_ZERO | ( | x | ) | ( ABSOLUTE_VALUE(x) < ZERO_EPSILON ) |
Definition at line 996 of file fsl_mpl3115_i2c_1D_press.c.
Referenced by fLfi().
| #define MPL3115_ALT_FIXED_CONVERSION_FACTOR 1 |
Definition at line 44 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_ALT_FIXED_CONVERSION_OFFSET 0 |
Definition at line 45 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_ALT_FLOAT_CONVERSION_FACTOR 1.0 |
Definition at line 42 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_ALT_FLOAT_CONVERSION_OFFSET 0.0 |
Definition at line 43 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_DEBUG 0 |
Definition at line 928 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_ONE_SECOND 1000000 |
Definition at line 154 of file fsl_mpl3115_i2c_1D_press.c.
Referenced by mpl3115_ValidateConfig().
| #define MPL3115_PRESS_FIXED_CONVERSION_FACTOR (1000/4) |
Definition at line 40 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_PRESS_FIXED_CONVERSION_OFFSET 0 |
Definition at line 41 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_PRESS_FLOAT_CONVERSION_FACTOR 0.000000061035 |
Definition at line 38 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_PRESS_FLOAT_CONVERSION_OFFSET 0.0 |
Definition at line 39 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_TEMP_FIXED_CONVERSION_FACTOR 256 |
Definition at line 48 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_TEMP_FIXED_CONVERSION_OFFSET 0 |
Definition at line 49 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_TEMP_FLOAT_CONVERSION_FACTOR 256.0 |
Definition at line 46 of file fsl_mpl3115_i2c_1D_press.c.
| #define MPL3115_TEMP_FLOAT_CONVERSION_OFFSET 0.0 |
Definition at line 47 of file fsl_mpl3115_i2c_1D_press.c.
| #define ZERO_EPSILON (1.0E-10) |
Definition at line 995 of file fsl_mpl3115_i2c_1D_press.c.
| anonymous enum |
| Enumerator | |
|---|---|
| LFI_NO_EXTRAPOLATION | |
| LFI_TABLE_LIMITS | |
| LFI_EXTRAPOLATE | |
Definition at line 51 of file fsl_mpl3115_i2c_1D_press.c.
| anonymous enum |
| Enumerator | |
|---|---|
| LFI_SUCCESS | |
| LFI_BAD_TABLE | |
| LFI_BAD_PTR | |
| LFI_OUT_OF_RANGE | |
Definition at line 57 of file fsl_mpl3115_i2c_1D_press.c.
| anonymous enum |
This enumerator describes the available sample rates for the MPL3115 accelerometer.
Definition at line 27 of file fsl_mpl3115_i2c_1D_press.h.
| anonymous enum |
This enumerator describes the available acceleration ranges for the MM865X family of accelerometers.
| Enumerator | |
|---|---|
| FSL_MPL3115_ACCEL_SCALE_2G |
select +/-2G range |
| FSL_MPL3115_ACCEL_SCALE_4G |
select +/-4G range |
| FSL_MPL3115_ACCEL_SCALE_8G |
select +/-8G range |
Definition at line 39 of file fsl_mpl3115_i2c_1D_press.h.
Definition at line 980 of file fsl_mpl3115_i2c_1D_press.c.
References fLfi().
Referenced by mpl3115_GetData().


| long fLfi | ( | const fLfiTable_t * | lookupTable, |
| float | lFiIn, | ||
| float * | lfiOut | ||
| ) |
Definition at line 997 of file fsl_mpl3115_i2c_1D_press.c.
References fLfiTable_t::dataPoints, fLfiTable_t::extrapolationBehavior, IS_PRACTICALLY_ZERO, LFI_BAD_PTR, LFI_BAD_TABLE, LFI_NO_EXTRAPOLATION, LFI_OUT_OF_RANGE, LFI_SUCCESS, LFI_TABLE_LIMITS, fLfiTable_t::maxIdx, dataPair_t::x, and dataPair_t::y.
Referenced by convertPressureToAltitude().

| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_Calibrate | ( | isf_SensorHandle_t * | pSensorHandle, |
| void * | pCalData | ||
| ) |
Definition at line 525 of file fsl_mpl3115_i2c_1D_press.c.
References ISF_SUCCESS.
| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_Configure | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 312 of file fsl_mpl3115_i2c_1D_press.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_register_periodic_callback(), DeviceDescriptor_struct::cDescriptor, isf_SensorHandle_st::controlData, DeviceDescriptor_struct::deviceSemaphore, dm_channel_acquire_lock(), dm_channel_release_lock(), DSA_ERR_CONFIGURE, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STOPPED, DSA_STATE_INITIALIZED, fsl_mpl3115_i2c_1D_press_PeriodicCallback(), ISF_SUCCESS, mpl3115_SetConfig(), mpl3115_SetMode(), isf_dsa_SensorSettings_st::nSamplePeriod, isf_SensorHandle_st::pDeviceDescriptor, SENSOR_STANDBY, isf_dsa_ControlData_st::sensorSettings, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_Convert | ( | volatile isf_SensorHandle_t * | pSensorHandle, |
| isf_SensorDataTypes_t | convertToType, | ||
| isf_dsa_result_types_t | resultType, | ||
| void * | pNativeSample, | ||
| void * | pConvertedSample, | ||
| int32 * | numBytes | ||
| ) |
This function coverts the raw sample data to the desired output type.
Definition at line 668 of file fsl_mpl3115_i2c_1D_press.c.
References DSA_ERR_BAD_RESULT_TYPE, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_RESULT_TYPE_ENG_FIXED, DSA_RESULT_TYPE_ENG_FLOAT, SensorConfig_st::pSensorSpecificSettings, isf_SensorHandle_st::pSensorStaticConfig, TYPE_ALTITUDE, TYPE_PRESSURE, and TYPE_TEMPERATURE.
Referenced by fsl_mpl3115_i2c_1D_press_PeriodicCallback().

| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_EndData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 461 of file fsl_mpl3115_i2c_1D_press.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_stop(), DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_END_DATA, DSA_ERR_PARAM, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, ISF_SUCCESS, mpl3115_SetMode(), isf_SensorHandle_st::pDeviceDescriptor, SENSOR_STANDBY, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_Initialize | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 191 of file fsl_mpl3115_i2c_1D_press.c.
References isf_SensorHandle_st::adapterStatus, mpl3115_DataBuffer_t::altitude, DeviceDescriptor_struct::cDescriptor, SensorConfig_st::channelId, COMM_STATE_OK, SensorConfig_st::commInfo, DeviceDescriptor_struct::deviceHandle, DeviceDescriptor_struct::deviceSemaphore, dm_channel_get_state(), dm_channel_init(), dm_channel_start(), dm_device_open(), DSA_ERR_INITIALIZE, DSA_ERR_PARAM, DSA_STATE_INITIALIZED, DSA_STATE_NOT_INITIALIZED, ISF_SUCCESS, mpl3115_CheckId(), DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, mpl3115_DataBuffer_t::pressure, isf_SensorHandle_st::pSensorStaticConfig, DeviceDescriptor_struct::skipFramecnt, mpl3115_DataBuffer_t::temperature, and mpl3115_DataBuffer_t::timestamp.

| void fsl_mpl3115_i2c_1D_press_PeriodicCallback | ( | void * | pSensorHandle | ) |
Definition at line 574 of file fsl_mpl3115_i2c_1D_press.c.
References isf_SensorHandle_st::adapterStatus, isf_SensorHandle_st::controlData, DeviceDescriptor_struct::deviceSemaphore, DSA_STATE_CONFIGURED_STARTED, fsl_mpl3115_i2c_1D_press_Convert(), isf_fifo_el_get_insert_pointer(), isf_fifo_el_increment(), ISF_FIFO_FULL, isf_fifo_lock(), isf_fifo_unlock(), isf_time_util_get_usec(), mpl3115_GetData(), isf_dsa_ControlData_st::nEventFieldIndex, DeviceDescriptor_struct::pCurrentSample, isf_SensorHandle_st::pDeviceDescriptor, isf_dsa_ControlData_st::pEventGroup, isf_dsa_SensorSettings_st::pSampleBufferInfo, isf_dsa_SensorSettings_st::resultFormat, isf_dsa_SensorSettings_st::resultType, isf_dsa_ControlData_st::sensorSettings, DeviceDescriptor_struct::skipFramecnt, mpl3115_DataBuffer_t::timestamp, and TYPE_NATIVE_SENSOR_DATA_TYPE.
Referenced by fsl_mpl3115_i2c_1D_press_Configure().


| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_Shutdown | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 545 of file fsl_mpl3115_i2c_1D_press.c.
References isf_SensorHandle_st::adapterStatus, bm_unregister_callback(), DSA_ERR_PARAM, DSA_STATE_INITIALIZED, ISF_SUCCESS, isf_SensorHandle_st::pDeviceDescriptor, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_StartData | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 401 of file fsl_mpl3115_i2c_1D_press.c.
References isf_SensorHandle_st::adapterStatus, BM_ERROR, bm_start(), DeviceDescriptor_struct::deviceSemaphore, DSA_ERR_PARAM, DSA_ERR_START_DATA, DSA_STATE_CONFIGURED_STARTED, DSA_STATE_CONFIGURED_STOPPED, FALSE, ISF_SUCCESS, mpl3115_SetMode(), isf_SensorHandle_st::pDeviceDescriptor, SENSOR_ACTIVE, and DeviceDescriptor_struct::token.

| isf_dsa_status_t fsl_mpl3115_i2c_1D_press_ValidateSettings | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pSensorSettings | ||
| ) |
Definition at line 283 of file fsl_mpl3115_i2c_1D_press.c.
References DSA_ERR_PARAM, and mpl3115_ValidateConfig().

| void mpl3115_CheckId | ( | int32_t * | status, |
| void * | pSensorHandle | ||
| ) |
This function validates the MPL3115 sensor is connected via the I2C bus.
Definition at line 798 of file fsl_mpl3115_i2c_1D_press.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_read(), ISF_SUCCESS, MPL3115_WHO_AM_I, MPL3115_WHOAMI_VALUE, isf_SensorHandle_st::pDeviceDescriptor, and SENSOR_ERROR_CHECKID.
Referenced by fsl_mpl3115_i2c_1D_press_Initialize().


| isf_dsa_status_t mpl3115_GetData | ( | isf_SensorHandle_t * | pSensorHandle, |
| mpl3115_DataBuffer_t * | pData | ||
| ) |
Definition at line 904 of file fsl_mpl3115_i2c_1D_press.c.
References mpl3115_DataBuffer_t::altitude, BYTES_FOR_FULL_READ, convertPressureToAltitude(), DeviceDescriptor_struct::deviceHandle, dm_device_read(), ISF_SUCCESS, MPL3115_OUT_P_MSB, isf_SensorHandle_st::pDeviceDescriptor, mpl3115_DataBuffer_t::pressure, SENSOR_ERROR_GETDATA, and mpl3115_DataBuffer_t::temperature.
Referenced by fsl_mpl3115_i2c_1D_press_PeriodicCallback().


| void mpl3115_ReadRegisters | ( | isf_SensorHandle_t * | pSensorHandle | ) |
Definition at line 931 of file fsl_mpl3115_i2c_1D_press.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_read(), MPL3115_OFF_H, MPL3115_WHO_AM_I, and isf_SensorHandle_st::pDeviceDescriptor.
Referenced by mpl3115_SetConfig().


| void mpl3115_Reset | ( | int32_t * | status, |
| void * | pSensorHandle | ||
| ) |
This function resets the MPL3115 sensor resulting in a default configuration for all registers.
Definition at line 773 of file fsl_mpl3115_i2c_1D_press.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_write(), DSA_ERR_INITIALIZE, ISF_SUCCESS, MPL3115_CTRL_REG1, MPL3115_RST_MASK, and isf_SensorHandle_st::pDeviceDescriptor.

| isf_dsa_status_t mpl3115_SetConfig | ( | isf_SensorHandle_t * | pSensorHandle, |
| isf_dsa_SensorSettings_t * | pConfigSettings | ||
| ) |
This function sets the MPL3115 sensor configuration.
Definition at line 948 of file fsl_mpl3115_i2c_1D_press.c.
References DeviceDescriptor_struct::deviceHandle, dm_device_write(), DSA_ERR_CONFIGURE, ISF_SUCCESS, MPL3115_CTRL_REG2, MPL3115_ERROR, mpl3115_ReadRegisters(), MPL3115_SET_FIELD, isf_SensorHandle_st::pDeviceDescriptor, SensorConfig_st::pSensorSpecificSettings, and isf_SensorHandle_st::pSensorStaticConfig.
Referenced by fsl_mpl3115_i2c_1D_press_Configure().


| void mpl3115_SetMode | ( | int32_t * | status, |
| void * | pSensorHandle, | ||
| int32_t | Mode | ||
| ) |
This function sets the MPL3115 part to the requested mode.
Definition at line 839 of file fsl_mpl3115_i2c_1D_press.c.
References DeviceDescriptor_struct::deviceHandle, and isf_SensorHandle_st::pDeviceDescriptor.
Referenced by fsl_mpl3115_i2c_1D_press_Configure(), fsl_mpl3115_i2c_1D_press_EndData(), and fsl_mpl3115_i2c_1D_press_StartData().

| void mpl3115_ValidateConfig | ( | int32_t * | status, |
| void * | pSensorHandle, | ||
| void * | pSettings | ||
| ) |
This function validates the configuration for the MPL3115 sensor.
Definition at line 821 of file fsl_mpl3115_i2c_1D_press.c.
References DSA_RET_SETTINGS_CHANGED, ISF_SUCCESS, MPL3115_ONE_SECOND, and isf_dsa_SensorSettings_st::nSamplePeriod.
Referenced by fsl_mpl3115_i2c_1D_press_ValidateSettings().

| isf_SensorDataTypes_t mpl3115_SupportedDataTypes[] |
Definition at line 157 of file fsl_mpl3115_i2c_1D_press.c.
| isf_SensorDataTypes_t mpl3115_SupportedDataTypes[] = { TYPE_TEMPERATURE, TYPE_ALTITUDE, TYPE_PRESSURE, TYPE_NATIVE_SENSOR_DATA_TYPE } |
Definition at line 157 of file fsl_mpl3115_i2c_1D_press.c.
| isf_SensorTypes_t mpl3115_SupportedSensorTypes[] |
Supported sensor and data types for MPL3115.
Definition at line 156 of file fsl_mpl3115_i2c_1D_press.c.
| isf_SensorTypes_t mpl3115_SupportedSensorTypes[] = { TYPE_THERMOMETER, TYPE_ALTIMETER, TYPE_BAROMETER, TYPE_ABSOLUTE_PRESSURE_SENSOR, TYPE_NATIVE_SENSOR_TYPE } |
Supported sensor and data types for MPL3115.
Definition at line 156 of file fsl_mpl3115_i2c_1D_press.c.