![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | PitUserConfig |
| PIT timer configuration structure. More... | |
Typedefs | |
| typedef struct PitUserConfig | pit_user_config_t |
| PIT timer configuration structure. More... | |
| typedef void(* | pit_isr_callback_t )(void) |
| PIT ISR callback function typedef. More... | |
Functions | |
| void | pit_init_module (bool isRunInDebug) |
| Initialize PIT module. More... | |
| void | pit_init_channel (uint32_t timer, const pit_user_config_t *config) |
| Initialize PIT channel. More... | |
| void | pit_shutdown (void) |
| Disable PIT module and gate control. More... | |
| void | pit_timer_start (uint32_t timer) |
| Start timer counting. More... | |
| void | pit_timer_stop (uint32_t timer) |
| Stop timer counting. More... | |
| void | pit_set_timer_period_us (uint32_t timer, uint32_t us) |
| Set timer period in microsecond units. More... | |
| uint32_t | pit_read_timer_us (uint32_t timer) |
| Read current timer value in microsecond units. More... | |
| void | pit_init (bool bEnableirq, uint32 usec) |
| Complete initialization of the PIT timer. More... | |
| void | pit_register_isr_callback_function (uint32_t timer, pit_isr_callback_t function) |
| Register pit isr callback function. More... | |
| typedef void(* pit_isr_callback_t)(void) |
PIT ISR callback function typedef.
Definition at line 45 of file fsl_pit_driver.h.
| typedef struct PitUserConfig pit_user_config_t |
PIT timer configuration structure.
Define structure PitConfig and use pit_init_channel() to make necessary initializations. You may also use remaining functions for PIT configuration.
Complete initialization of the PIT timer.
Definition at line 201 of file fsl_pit_driver.c.
References FALSE, ISF_BM_PIT_INSTANCE, PitUserConfig::isInterruptEnabled, pit_hal_clear_interrupt_flag(), pit_init_channel(), pit_init_module(), pit_set_timer_period_us(), and pit_timer_stop().
Referenced by bm_timer_init().


| void pit_init_channel | ( | uint32_t | timer, |
| const pit_user_config_t * | config | ||
| ) |
Initialize PIT channel.
This function initialize PIT timers by channel. Pass in timer number and its config structure. Timers do not start counting by default after calling this function. Function pit_timer_start must be called to start timer counting. Call pit_set_timer_period_us to re-set the period.
Here is an example demonstrating how to define a PIT channel config structure:
| timer | Timer channel number. |
| config | PIT channel configuration structure. |
Definition at line 69 of file fsl_pit_driver.c.
References TU_instance_PEx_t::fnTULDDInit, PitUserConfig::isInterruptEnabled, PitUserConfig::periodUs, pit_hal_configure_interrupt(), pit_set_timer_period_us(), and TU_instance_tbl.
Referenced by bm_start(), bm_timer_init(), and pit_init().


| void pit_init_module | ( | bool | isRunInDebug | ) |
Initialize PIT module.
This function must be called before calling all the other PIT driver functions. This function un-gates the PIT clock and enables the PIT module. The isRunInDebug passed into function will affect all timer channels.
| isRunInDebug | Timers run or stop in debug mode.
|
Definition at line 46 of file fsl_pit_driver.c.
References BM_PIT_SOURCE_CLK, pit_hal_configure_timer_run_in_debug(), pit_hal_enable(), and pitSourceClock.
Referenced by bm_start(), bm_timer_init(), and pit_init().


| uint32_t pit_read_timer_us | ( | uint32_t | timer | ) |
Read current timer value in microsecond units.
This function returns an absolute time stamp in microsecond units. One common use of this function is to measure the running time of a part of code. Call this function at both the beginning and end of code; the time difference between these two time stamps is the running time (Make sure the running time will not exceed the timer period). The time stamp returned is up-counting.
| timer | Timer channel number. |
Definition at line 150 of file fsl_pit_driver.c.
References pit_hal_read_timer_count(), and pitSourceClock.

| void pit_register_isr_callback_function | ( | uint32_t | timer, |
| pit_isr_callback_t | function | ||
| ) |
Register pit isr callback function.
System default ISR interfaces are already defined in fsl_pit_irq.c. Users can either edit these ISRs or use this function to register a callback function. The default ISR runs the callback function if there is one installed.
| timer | Timer channel number. |
| function | Pointer to pit isr callback function. |
Definition at line 160 of file fsl_pit_irq.c.
References pit_isr_callback_table.
| void pit_set_timer_period_us | ( | uint32_t | timer, |
| uint32_t | us | ||
| ) |
Set timer period in microsecond units.
The period range depends on the frequency of PIT source clock. If the required period is out of range, use the lifetime timer, if applicable.
| timer | Timer channel number. |
| us | Timer period in microseconds. |
Definition at line 131 of file fsl_pit_driver.c.
References BM_PIT_SCALER, and pit_hal_set_timer_period_count().
Referenced by bm_start(), bm_timer_init(), isr_bm_callback_tmr(), pit_init(), and pit_init_channel().


| void pit_shutdown | ( | void | ) |
Disable PIT module and gate control.
This function disables all PIT interrupts and PIT clock. It then gates the PIT clock control. pit_init_module must be called if you want to use PIT again.
Definition at line 90 of file fsl_pit_driver.c.
References pit_hal_disable().

| void pit_timer_start | ( | uint32_t | timer | ) |
Start timer counting.
After calling this function, timers load period value, count down to 0 and then load the respective start value again. Each time a timer reaches 0, it generates a trigger pulse and sets the timeout interrupt flag.
| timer | Timer channel number. |
Definition at line 105 of file fsl_pit_driver.c.
References pit_hal_timer_start().
Referenced by bm_start().


| void pit_timer_stop | ( | uint32_t | timer | ) |
Stop timer counting.
This function stops every timer counting. Timers reload their periods respectively after the next time they call pit_timer_start.
| timer | Timer channel number. |
Definition at line 118 of file fsl_pit_driver.c.
References pit_hal_timer_stop().
Referenced by bm_powerdown(), bm_start(), bm_timer_init(), and pit_init().