![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Data Structures | |
| struct | rliConfigRegister_t |
| struct | rliAppStatus_t |
| rli application configuration buffer format. More... | |
| struct | rliAppState_t |
| struct | device_cmd_packet_t |
| rli overall application state buffer format. More... | |
Macros | |
| #define | MQX_DISABLE_CONFIG_CHECK 1 |
| #define | SENSOR_DATA_READY_EVENT ((uint32)(1 << 10)) |
| #define | RLI_COMM_BUFFER_SIZE (255) |
| #define | SET_FIELD(name, val) (((val)<<name##_SHIFT)&(name##_MASK)) |
| Macro that extracts one of the fields below. More... | |
| #define | GET_FIELD(name, val) ((val&name##_MASK)>>name##_SHIFT) |
Enumerations | |
| enum | { CI_CMD_DEVICE_WRITE = (CI_CMD_RESET_APP+1), CI_CMD_DEVICE_READ } |
| enum | { RLI_APP_STATE_CLOSED = 0, RLI_APP_STATE_OPEN = 1, RLI_APP_STATE_ERROR = 0xFF } |
| enum | { FSL_RLI_APP_ID = 2 } |
Functions | |
| ci_response_t | rli_ci_app_callback (ci_host_cmd_packet_t *pHostPacket, ci_app_resp_packet_t *pAppPacket) |
| void | rli_app_task (void) |
| int32 | open_channel (rliAppState_t *appState) |
| int32 | close_channel (rliAppState_t *appState) |
| int32 | device_connect (rliAppState_t *appState) |
| int32 | device_disconnect (rliAppState_t *appState) |
Variables | |
| uint8_t | rcvBuffer_t [RLI_COMM_BUFFER_SIZE] |
| uint8_t | cmdBuffer_t [RLI_COMM_BUFFER_SIZE] |
| MQX_INITIALIZATION_STRUCT | MQX_init_struct |
| This data structure/variable holds the complete state of the rli magnetometer sensor embedded application. More... | |
| #define GET_FIELD | ( | name, | |
| val | |||
| ) | ((val&name##_MASK)>>name##_SHIFT) |
Definition at line 60 of file rli_project.c.
| #define MQX_DISABLE_CONFIG_CHECK 1 |
Definition at line 18 of file rli_project.c.
| #define RLI_COMM_BUFFER_SIZE (255) |
Definition at line 43 of file rli_project.c.
| #define SENSOR_DATA_READY_EVENT ((uint32)(1 << 10)) |
Definition at line 42 of file rli_project.c.
| #define SET_FIELD | ( | name, | |
| val | |||
| ) | (((val)<<name##_SHIFT)&(name##_MASK)) |
Macro that extracts one of the fields below.
Definition at line 59 of file rli_project.c.
| anonymous enum |
| Enumerator | |
|---|---|
| CI_CMD_DEVICE_WRITE | |
| CI_CMD_DEVICE_READ | |
Definition at line 47 of file rli_project.c.
| anonymous enum |
| Enumerator | |
|---|---|
| RLI_APP_STATE_CLOSED | |
| RLI_APP_STATE_OPEN | |
| RLI_APP_STATE_ERROR | |
Definition at line 52 of file rli_project.c.
| anonymous enum |
| Enumerator | |
|---|---|
| FSL_RLI_APP_ID | |
Definition at line 104 of file rli_project.c.
| int32 close_channel | ( | rliAppState_t * | appState | ) |
Definition at line 352 of file rli_project.c.
References rliAppStatus_t::channel, isf_rli_deint(), rliAppState_t::pChannelDescriptor, RLI_APP_STATE_CLOSED, RLI_APP_STATE_ERROR, and rliAppState_t::status.
Referenced by rli_ci_app_callback().


| int32 device_connect | ( | rliAppState_t * | appState | ) |
Definition at line 313 of file rli_project.c.
References I2CDeviceInfo::address, rliAppState_t::CfgBuffer, rliAppStatus_t::device, rliConfigRegister_t::deviceAddress, isf_rli_open(), rliAppState_t::pChannelDescriptor, rliAppState_t::pHandle, RLI_APP_STATE_ERROR, RLI_APP_STATE_OPEN, and rliAppState_t::status.
Referenced by rli_app_task(), and rli_ci_app_callback().


| int32 device_disconnect | ( | rliAppState_t * | appState | ) |
Definition at line 326 of file rli_project.c.
References rliAppStatus_t::device, isf_rli_close(), rliAppState_t::pHandle, RLI_APP_STATE_CLOSED, RLI_APP_STATE_ERROR, and rliAppState_t::status.
Referenced by rli_ci_app_callback().


| int32 open_channel | ( | rliAppState_t * | appState | ) |
Definition at line 338 of file rli_project.c.
References rliAppState_t::CfgBuffer, rliAppStatus_t::channel, rliConfigRegister_t::channelID, isf_rli_init(), rliAppState_t::pChannelDescriptor, RLI_APP_STATE_ERROR, RLI_APP_STATE_OPEN, and rliAppState_t::status.
Referenced by rli_ci_app_callback().


| void rli_app_task | ( | void | ) |
Definition at line 127 of file rli_project.c.
References rliAppState_t::CfgBuffer, rliConfigRegister_t::channelID, COMM_CHANNEL_I2C_CH1, device_connect(), rliConfigRegister_t::deviceAddress, isf_rli_init(), and rliAppState_t::pChannelDescriptor.
Referenced by TaskRLI1_task().


| ci_response_t rli_ci_app_callback | ( | ci_host_cmd_packet_t * | pHostPacket, |
| ci_app_resp_packet_t * | pAppPacket | ||
| ) |
Definition at line 151 of file rli_project.c.
References device_cmd_packet_t::appId, ci_host_cmd_packet_t::appId, ci_host_cmd_packet_t::byte_cnt, ci_app_resp_packet_t::bytes_xfer, rliAppState_t::CfgBuffer, rliAppStatus_t::channel, CI_CMD_DEVICE_READ, CI_CMD_DEVICE_WRITE, CI_CMD_READ_APP_DATA, CI_CMD_READ_APP_STATUS, CI_CMD_READ_CONFIG, CI_CMD_RESET_APP, CI_CMD_UPDATE_QUICKREAD, CI_CMD_WRITE_CONFIG, CI_ERROR_COMMAND, CI_ERROR_NONE, CI_INVALID_COUNT, CI_RW_READ, CI_RW_WRITE, close_channel(), device_cmd_packet_t::cmd, ci_host_cmd_packet_t::cmd, rliAppState_t::cmdBuffer, cmdBuffer_t, rliAppStatus_t::device, device_connect(), device_disconnect(), rliAppStatus_t::error, FSL_RLI_APP_ID, isf_ci_app_read(), isf_ci_app_write(), isf_ci_qr_update(), isf_rli_read(), isf_rli_write(), ISF_SUCCESS, device_cmd_packet_t::nRead, device_cmd_packet_t::nWrite, ci_host_cmd_packet_t::offset, open_channel(), rliAppState_t::pHandle, rliAppState_t::rcvBuffer, rcvBuffer_t, RLI_APP_STATE_OPEN, ci_app_resp_packet_t::rw, and rliAppState_t::status.

| uint8_t cmdBuffer_t[RLI_COMM_BUFFER_SIZE] |
Definition at line 45 of file rli_project.c.
Referenced by rli_ci_app_callback().
| MQX_INITIALIZATION_STRUCT MQX_init_struct |
| uint8_t rcvBuffer_t[RLI_COMM_BUFFER_SIZE] |
Definition at line 44 of file rli_project.c.
Referenced by rli_ci_app_callback().