![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
isf_comm.h defines the common types for the Communications Service Family of the Intelligent Sensing Framework (ISF). More...
#include <isf.h>

Go to the source code of this file.
Typedefs | |
| typedef uint32 | comm_Id_t |
| This type is for a numeric channel identifier- index into an array of channels in the system. More... | |
| typedef enum comm_State_vals | comm_State_t |
| This enum holds an enumerated value describing the state of a channel. More... | |
| typedef uint32 | comm_Address_t |
| This type is for a channel address for both 7-bit and 10-bit addresses. More... | |
| typedef uint8 | comm_Flags_t |
| This is a bit array of flags governing device read/write behavior. More... | |
Enumerations | |
| enum | comm_State_vals { COMM_STATE_NO_INIT = 0, COMM_STATE_INIT = 1, COMM_STATE_OK = 2, COMM_STATE_STOPPED = 3, COMM_STATE_ERROR = 5, COMM_STATE_ARB_LOST = 6 } |
| This enum defines the possible communications channel states. More... | |
| enum | comm_Error_vals { COMM_ERROR_INIT = 1, COMM_ERROR_STOP = 2, COMM_ERROR_LOCK = 3, COMM_ERROR_TIME_OUT = 4, COMM_ERROR_NULL_PTR = 5, COMM_ERROR_NOEXIST = 6, COMM_ERROR_BUF_SIZE = 7, COMM_ERROR_NO_ACK = 8, COMM_ERROR_DEV_CLOSED = 9, COMM_ERROR_OTHER = 10 } |
| This enum defines the possible communications channel error codes. More... | |
isf_comm.h defines the common types for the Communications Service Family of the Intelligent Sensing Framework (ISF).
File: isf_comm.h
Copyright (c) 2012, Freescale Semiconductor, Inc.
This common types used by components in the ISF Communications Service Family, including the I2C and Device Messaging Components. Since the Device Messaging Component abstracts various communications interfaces (I2C, SPI, RGPIO), it is important to ensure that all abstracted components use common data types and function prototypes. These types and prototypes are defined in the header file rather than in the Device Messaging header file to avoid creating a circular dependency.
Definition in file isf_comm.h.
| typedef uint32 comm_Address_t |
This type is for a channel address for both 7-bit and 10-bit addresses.
Definition at line 56 of file isf_comm.h.
| typedef uint8 comm_Flags_t |
This is a bit array of flags governing device read/write behavior.
Definition at line 59 of file isf_comm.h.
This type is for a numeric channel identifier- index into an array of channels in the system.
Definition at line 50 of file isf_comm.h.
| typedef enum comm_State_vals comm_State_t |
This enum holds an enumerated value describing the state of a channel.
Definition at line 53 of file isf_comm.h.
| enum comm_Error_vals |
This enum defines the possible communications channel error codes.
Definition at line 35 of file isf_comm.h.
| enum comm_State_vals |
This enum defines the possible communications channel states.
Definition at line 25 of file isf_comm.h.