![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "isf_target.h"#include "isf_types.h"#include "lwevent.h"#include "isf_sysconf_types.h"#include "isf_sensor_types.h"#include "isf_fifo.h"

Go to the source code of this file.
Data Structures | |
| struct | isf_dsa_DeviceInfoBlock_st |
| This defines the DSA adapter device information block. More... | |
| struct | isf_dsa_SensorSettings_st |
| This defines the DSA sensor configuration parameter structure configuring the sensor settings by a subscriber task. More... | |
| struct | isf_dsa_ControlData_st |
| This defines the DSA adapter functional interface. More... | |
| struct | isf_SensorHandle_st |
| This defines the DSA sensor device handle structure used to invoke the adapter access functions. More... | |
| struct | isf_dsa_info_t |
| struct | isf_dsa_ControlInterface_st |
| This defines the DSA adapter control interface abstract function list. More... | |
| struct | isf_dsa_Adapter_st |
| This defines the DSA adapter structure required for static initialization of the concrete instance of a given sensor adapter. More... | |
| struct | SensorConfig_st |
| This defines the DSA sensor configuration structure defining each individual sensor adapter in the DSA Sensor List. More... | |
Typedefs | |
| typedef int32 | isf_dsa_status_t |
| This is the Sensor Manager API return type definition. More... | |
| typedef enum isf_dsa_error_enums | isf_dsa_err_t |
| This enumerates the error types returned by the DSA sensor functions. More... | |
| typedef enum isf_dsa_result_enums | isf_dsa_result_types_t |
| typedef enum isf_dsa_AdapterStatus_enums | isf_dsa_AdapterStatus_t |
| This defines the standard DSA adapter sensor status types. User defined sensor adapters may need additional or different states. More... | |
| typedef struct isf_dsa_DeviceInfoBlock_st | isf_dsa_DeviceInfoBlock_t |
| This defines the DSA adapter device information block. More... | |
| typedef struct isf_dsa_SensorSettings_st | isf_dsa_SensorSettings_t |
| This defines the DSA sensor configuration parameter structure configuring the sensor settings by a subscriber task. More... | |
| typedef struct isf_dsa_ControlData_st | isf_dsa_ControlData_t |
| This defines the DSA adapter functional interface. More... | |
| typedef struct SensorConfig_st | isf_SensorConfig_t |
| typedef struct isf_SensorHandle_st | isf_SensorHandle_t |
| This defines the DSA sensor device handle structure used to invoke the adapter access functions. More... | |
| typedef isf_dsa_status_t( | isf_dsa_data_converter_t )(volatile isf_SensorHandle_t *, isf_SensorDataTypes_t, isf_dsa_result_types_t, void *, void *, int32 *numBytes) |
| typedef struct isf_dsa_ControlInterface_st | isf_dsa_ControlInterface_t |
| This defines the DSA adapter control interface abstract function list. More... | |
| typedef struct isf_dsa_Adapter_st | isf_dsa_Adapter_t |
| This defines the DSA adapter structure required for static initialization of the concrete instance of a given sensor adapter. More... | |
Enumerations | |
| enum | isf_dsa_error_enums { DSA_ERR_INITIALIZE = 1, DSA_ERR_VALIDATE_SETTINGS, DSA_ERR_CONFIGURE, DSA_ERR_START_DATA, DSA_ERR_END_DATA, DSA_ERR_CALIBRATE, DSA_ERR_SHUTDOWN, DSA_ERR_PARAM, DSA_ERR_NO_MEM, DSA_ERR_BAD_SENSOR_DATA_TYPE, DSA_ERR_BAD_RESULT_TYPE, DSA_RET_SETTINGS_CHANGED, DSA_FIFO_FULL } |
| This enumerates the error types returned by the DSA sensor functions. More... | |
| enum | isf_dsa_result_enums { DSA_RESULT_TYPE_RAW_COUNTS = 1, DSA_RESULT_TYPE_ENG_FIXED = 2, DSA_RESULT_TYPE_ENG_FLOAT = 3 } |
| enum | isf_dsa_AdapterStatus_enums { DSA_STATE_NOT_INITIALIZED = 0, DSA_STATE_INITIALIZED = 1, DSA_STATE_CONFIGURED_STOPPED = 2, DSA_STATE_CONFIGURED_STARTED = 3 } |
| This defines the standard DSA adapter sensor status types. User defined sensor adapters may need additional or different states. More... | |
| typedef struct isf_dsa_Adapter_st isf_dsa_Adapter_t |
This defines the DSA adapter structure required for static initialization of the concrete instance of a given sensor adapter.
| typedef enum isf_dsa_AdapterStatus_enums isf_dsa_AdapterStatus_t |
This defines the standard DSA adapter sensor status types. User defined sensor adapters may need additional or different states.
| typedef struct isf_dsa_ControlData_st isf_dsa_ControlData_t |
This defines the DSA adapter functional interface.
| typedef struct isf_dsa_ControlInterface_st isf_dsa_ControlInterface_t |
This defines the DSA adapter control interface abstract function list.
| typedef isf_dsa_status_t( isf_dsa_data_converter_t)(volatile isf_SensorHandle_t *, isf_SensorDataTypes_t, isf_dsa_result_types_t, void *, void *, int32 *numBytes) |
Definition at line 122 of file isf_dsa_adapter.h.
| typedef struct isf_dsa_DeviceInfoBlock_st isf_dsa_DeviceInfoBlock_t |
This defines the DSA adapter device information block.
| typedef enum isf_dsa_error_enums isf_dsa_err_t |
This enumerates the error types returned by the DSA sensor functions.
| typedef enum isf_dsa_result_enums isf_dsa_result_types_t |
| typedef struct isf_dsa_SensorSettings_st isf_dsa_SensorSettings_t |
This defines the DSA sensor configuration parameter structure configuring the sensor settings by a subscriber task.
| typedef int32 isf_dsa_status_t |
This is the Sensor Manager API return type definition.
Definition at line 23 of file isf_dsa_adapter.h.
| typedef struct SensorConfig_st isf_SensorConfig_t |
Definition at line 103 of file isf_dsa_adapter.h.
| typedef struct isf_SensorHandle_st isf_SensorHandle_t |
This defines the DSA sensor device handle structure used to invoke the adapter access functions.
This defines the standard DSA adapter sensor status types. User defined sensor adapters may need additional or different states.
| Enumerator | |
|---|---|
| DSA_STATE_NOT_INITIALIZED | |
| DSA_STATE_INITIALIZED | |
| DSA_STATE_CONFIGURED_STOPPED | |
| DSA_STATE_CONFIGURED_STARTED | |
Definition at line 58 of file isf_dsa_adapter.h.
| enum isf_dsa_error_enums |
This enumerates the error types returned by the DSA sensor functions.
Definition at line 29 of file isf_dsa_adapter.h.
| enum isf_dsa_result_enums |
| Enumerator | |
|---|---|
| DSA_RESULT_TYPE_RAW_COUNTS | |
| DSA_RESULT_TYPE_ENG_FIXED | |
| DSA_RESULT_TYPE_ENG_FLOAT | |
Definition at line 47 of file isf_dsa_adapter.h.