![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|


Go to the source code of this file.
Data Structures | |
| struct | isf_SubscriptionSettings_t |
Macros | |
| #define | ERR_INVALID_HANDLE (int32)(-1L) |
| #define | ERR_INVALID_PTR (int32)(-2L) |
| #define ERR_INVALID_HANDLE (int32)(-1L) |
Error Return codes
Definition at line 18 of file isf_dsa_direct_types.h.
Referenced by init_sensor().
| #define ERR_INVALID_PTR (int32)(-2L) |
Definition at line 19 of file isf_dsa_direct_types.h.
Referenced by init_sensor().