![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|

Go to the source code of this file.
Macros | |
| #define | ALLOCATED_BUFFER_BIT ((uint8)(1<<0)) |
| #define | FIFO_FULL_BIT ((uint8)(1<<7)) |
| #define | FIFO_FULL_CLR_MASK ((uint8)~FIFO_FULL_BIT) |
Functions | |
| isf_fifo_status_t | isf_fifo_init (isf_fifo_t *pFifo, void *pData, uint16 sampleSize, uint16 bufferCapacity) |
| Initializes a new fifo structure with a provided buffer. More... | |
| isf_fifo_status_t | isf_fifo_alloc (isf_fifo_t *pFifo, uint16 sampleSize, uint16 bufferCapacity) |
| Convenience function to initialize a fifo structure and allocate a new fifo buffer. More... | |
| isf_fifo_status_t | isf_fifo_free (isf_fifo_t *pFifo) |
| free a fifo's sample buffer. More... | |
| isf_fifo_status_t | isf_fifo_resize (isf_fifo_t *pFifo, uint16 newCapacity) |
| Routine to change the supported fifo depth. More... | |
| uint16 | isf_fifo_get_buffer_size (isf_fifo_t *pFifo) |
| Routine to query the current fifo buffer size (bytes) More... | |
| isf_fifo_status_t | isf_fifo_data_copy (isf_fifo_t *pFifo, void *samplePtr) |
| Routine to copy the whole sample buffer. More... | |
| isf_fifo_status_t | isf_fifo_lock (isf_fifo_t *pFifo) |
| Lock a sample buffer for exclusive access. More... | |
| isf_fifo_status_t | isf_fifo_try_lock (isf_fifo_t *pFifo) |
| Attempt to lock a sample buffer for exclusive access. More... | |
| isf_fifo_status_t | isf_fifo_unlock (isf_fifo_t *pFifo) |
| Release the exclusive access lock on a sample buffer. More... | |
| isf_fifo_status_t | isf_fifo_el_clear (isf_fifo_t *pFifo) |
| Routine to clear the fifo. More... | |
| void * | isf_fifo_el_get_insert_pointer (isf_fifo_t *pFifo) |
| Routine returns the insert pointer for direct access. More... | |
| isf_fifo_status_t | isf_fifo_el_increment (isf_fifo_t *pFifo) |
| Routine increments the insert pointer after direct access. More... | |
| isf_fifo_status_t | isf_fifo_el_traverse (isf_fifo_t *pFifo, void **pSamplePtr) |
| Routine to traverse a fifo To initiate the traversal set pSamplePtr to NULL. The function will set the pointer to the first available sample and returns ISF_SUCCESS. Subsequent calls will increment the pointer to each available sample and return ISF_SUCCESS. When ISF_SUCCESS is returned, pSamplePtr may be dereferenced to obtain a fifo entry. When no more samples are available, the function returns ISF_FIFO_NO_MORE_ENTRIES. More... | |
| #define ALLOCATED_BUFFER_BIT ((uint8)(1<<0)) |
Definition at line 12 of file isf_fifo.c.
Referenced by isf_fifo_free(), isf_fifo_init(), and isf_fifo_resize().
| #define FIFO_FULL_BIT ((uint8)(1<<7)) |
Definition at line 13 of file isf_fifo.c.
Referenced by isf_fifo_el_increment(), and isf_fifo_el_traverse().
| #define FIFO_FULL_CLR_MASK ((uint8)~FIFO_FULL_BIT) |
Definition at line 14 of file isf_fifo.c.
Referenced by isf_fifo_el_clear().
| isf_fifo_status_t isf_fifo_alloc | ( | isf_fifo_t * | pFifo, |
| uint16 | sampleSize, | ||
| uint16 | bufferCapacity | ||
| ) |
Convenience function to initialize a fifo structure and allocate a new fifo buffer.
Initializes a fifo structure and allocates a new fifo buffer.
Definition at line 69 of file isf_fifo.c.
References isf_fifo_init().

| isf_fifo_status_t isf_fifo_data_copy | ( | isf_fifo_t * | pFifo, |
| void * | samplePtr | ||
| ) |
Routine to copy the whole sample buffer.
Definition at line 155 of file isf_fifo.c.
References isf_fifo_t::bufferLock, ISF_FIFO_ERR_NO_INIT, isf_mem_copy(), ISF_SUCCESS, isf_fifo_t::pDataBuffer, and isf_fifo_t::pLastEntry.

| isf_fifo_status_t isf_fifo_el_clear | ( | isf_fifo_t * | pFifo | ) |
Routine to clear the fifo.
Definition at line 220 of file isf_fifo.c.
References FIFO_FULL_CLR_MASK, isf_fifo_t::fifoState, ISF_SUCCESS, isf_fifo_t::pDataBuffer, and isf_fifo_t::pInsertPtr.
Referenced by App1_MainTask(), and fsl_fusion_virt_3D_orient_PeriodicCallback().

| void* isf_fifo_el_get_insert_pointer | ( | isf_fifo_t * | pFifo | ) |
Routine returns the insert pointer for direct access.
Definition at line 232 of file isf_fifo.c.
References isf_fifo_t::pInsertPtr.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().

| isf_fifo_status_t isf_fifo_el_increment | ( | isf_fifo_t * | pFifo | ) |
Routine increments the insert pointer after direct access.
Definition at line 240 of file isf_fifo.c.
References FIFO_FULL_BIT, isf_fifo_t::fifoState, ISF_FIFO_FULL, ISF_SUCCESS, isf_fifo_t::pInsertPtr, isf_fifo_t::pLastEntry, and isf_fifo_t::sampleSize.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().

| isf_fifo_status_t isf_fifo_el_traverse | ( | isf_fifo_t * | pFifo, |
| void ** | pSamplePtr | ||
| ) |
Routine to traverse a fifo To initiate the traversal set pSamplePtr to NULL. The function will set the pointer to the first available sample and returns ISF_SUCCESS. Subsequent calls will increment the pointer to each available sample and return ISF_SUCCESS. When ISF_SUCCESS is returned, pSamplePtr may be dereferenced to obtain a fifo entry. When no more samples are available, the function returns ISF_FIFO_NO_MORE_ENTRIES.
Definition at line 262 of file isf_fifo.c.
References FIFO_FULL_BIT, isf_fifo_t::fifoState, ISF_FIFO_NO_MORE_ENTRIES, ISF_SUCCESS, isf_fifo_t::pDataBuffer, isf_fifo_t::pInsertPtr, and isf_fifo_t::sampleSize.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback().

| isf_fifo_status_t isf_fifo_free | ( | isf_fifo_t * | pFifo | ) |
free a fifo's sample buffer.
Definition at line 77 of file isf_fifo.c.
References ALLOCATED_BUFFER_BIT, isf_fifo_t::bufferLock, isf_fifo_t::fifoState, ISF_FIFO_ERR_NO_INIT, ISF_SUCCESS, isf_fifo_t::pDataBuffer, isf_fifo_t::pInsertPtr, and isf_fifo_t::pLastEntry.
| uint16 isf_fifo_get_buffer_size | ( | isf_fifo_t * | pFifo | ) |
Routine to query the current fifo buffer size (bytes)
Routine to query the current fifo size (bytes)
Definition at line 134 of file isf_fifo.c.
References isf_fifo_t::pDataBuffer, isf_fifo_t::pLastEntry, and isf_fifo_t::sampleSize.
Referenced by isf_fifo_resize().

| isf_fifo_status_t isf_fifo_init | ( | isf_fifo_t * | pFifo, |
| void * | pData, | ||
| uint16 | sampleSize, | ||
| uint16 | bufferCapacity | ||
| ) |
Initializes a new fifo structure with a provided buffer.
Definition at line 19 of file isf_fifo.c.
References ALLOCATED_BUFFER_BIT, isf_fifo_t::bufferLock, isf_fifo_t::fifoState, ISF_FIFO_ERR_INVALID_PTR, ISF_FIFO_ERR_NO_INIT, ISF_FIFO_ERR_NO_MEM, isf_fifo_t::pDataBuffer, isf_fifo_t::pInsertPtr, isf_fifo_t::pLastEntry, and isf_fifo_t::sampleSize.
Referenced by App1_MainTask(), fsl_fusion_virt_3D_orient_Configure(), and isf_fifo_alloc().

| isf_fifo_status_t isf_fifo_lock | ( | isf_fifo_t * | pFifo | ) |
Lock a sample buffer for exclusive access.
Definition at line 171 of file isf_fifo.c.
References isf_fifo_t::bufferLock, ISF_FIFO_ERR_NO_INIT, and ISF_SUCCESS.
Referenced by App1_MainTask(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().

| isf_fifo_status_t isf_fifo_resize | ( | isf_fifo_t * | pFifo, |
| uint16 | newCapacity | ||
| ) |
Routine to change the supported fifo depth.
Routine to copy the whole sample buffer.
Warning: When the fifo is resized all sample data in the buffer is lost. It is suggested to resize only when empty
Definition at line 101 of file isf_fifo.c.
References ALLOCATED_BUFFER_BIT, isf_fifo_t::bufferLock, isf_fifo_t::fifoState, ISF_FIFO_ERR_NO_INIT, ISF_FIFO_ERR_USER_BUF, isf_fifo_get_buffer_size(), ISF_SUCCESS, isf_fifo_t::pDataBuffer, and isf_fifo_t::sampleSize.

| isf_fifo_status_t isf_fifo_try_lock | ( | isf_fifo_t * | pFifo | ) |
Attempt to lock a sample buffer for exclusive access.
Definition at line 184 of file isf_fifo.c.
References isf_fifo_t::bufferLock, ISF_FIFO_ERR_BUSY, ISF_SUCCESS, and TRUE.
| isf_fifo_status_t isf_fifo_unlock | ( | isf_fifo_t * | pFifo | ) |
Release the exclusive access lock on a sample buffer.
Definition at line 202 of file isf_fifo.c.
References isf_fifo_t::bufferLock, ISF_FIFO_ERR_NO_INIT, and ISF_SUCCESS.
Referenced by App1_MainTask(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().