![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
isf_fsl_spi_master_PEx.c implements PEx properties and event. Its also implements LDD overriding events. More...
#include "isf_fsl_spi_master_PEx.h"#include "mqxlite.h"#include "lwevent.h"#include "fsl_spi_master_driver.h"#include "isf_spi_master_adapter.h"#include "SPIMasterBus1.h"
Go to the source code of this file.
Variables | |
| const spi_master_instance_PEx | spi_master_instance_tbl [] |
| Lookup table for the LLD instance. More... | |
isf_fsl_spi_master_PEx.c implements PEx properties and event. Its also implements LDD overriding events.
isf_fsl_spi_master_PEx
Copyright (c) 2012-2014, Freescale Semiconductor, Inc.
Definition in file isf_fsl_spi_master_PEx.c.
| const spi_master_instance_PEx spi_master_instance_tbl[] |
Lookup table for the LLD instance.
Definition at line 26 of file isf_fsl_spi_master_PEx.c.