![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "PE_Types.h"

Go to the source code of this file.
Data Structures | |
| struct | uart_instance_PEx |
| This structure contains i2c LLD function pointers. More... | |
Typedefs | |
| typedef LDD_TDeviceData *(* | fnUARTInit_t )(LDD_TUserData *apUserData) |
| This is the function pointer signature for i2c initialization. More... | |
| typedef LDD_TError(* | fnUARTRead_t )(LDD_TDeviceData *apDevice, LDD_TData *BufferPtr, uint16_t Size) |
| This is the function pointer signature for reading the data from a specified device. More... | |
| typedef LDD_TError(* | fnUARTWrite_t )(LDD_TDeviceData *apDevice, LDD_TData *BufferPtr, uint16_t Size) |
| This is the the function pointer signature for writing the data to a specified device. More... | |
| typedef LDD_TDeviceData*(* fnUARTInit_t)(LDD_TUserData *apUserData) |
This is the function pointer signature for i2c initialization.
Definition at line 14 of file isf_fsl_uart_PEx.h.
| typedef LDD_TError(* fnUARTRead_t)(LDD_TDeviceData *apDevice, LDD_TData *BufferPtr, uint16_t Size) |
This is the function pointer signature for reading the data from a specified device.
Definition at line 18 of file isf_fsl_uart_PEx.h.
| typedef LDD_TError(* fnUARTWrite_t)(LDD_TDeviceData *apDevice, LDD_TData *BufferPtr, uint16_t Size) |
This is the the function pointer signature for writing the data to a specified device.
Definition at line 22 of file isf_fsl_uart_PEx.h.