![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
isf_protocol_adapter.h defines the general interface definition for the protocol adapter. More...


Go to the source code of this file.
Data Structures | |
| struct | protocol_t |
| This structure contains protocol-specific function pointers and properties. More... | |
| struct | busHandle_struct |
| This structure is a declaration of a BusHandle type. More... | |
Typedefs | |
| typedef isf_status_t(* | fnInit_t )(comm_Id_t aBusId, void *apBusHandle) |
| This is the function pointer signature for bus initialization. More... | |
| typedef comm_State_t(* | fnGetState_t )(void *apBusHandle) |
| This is the function pointer signature for getting the state of the bus. More... | |
| typedef isf_status_t(* | fnGetConfig_t )(void *apBusHandle, void *apBusConfig) |
| This is the function pointer signature for getting the configuration of the bus. More... | |
| typedef isf_status_t(* | fnConfigure_t )(void *apBusHandle, void *apBusConfig) |
| This is the function pointer signature for setting the configuration of the bus. More... | |
| typedef isf_status_t(* | fnStart_t )(void *apBusHandle) |
| This is the function pointer signature for starting the bus. More... | |
| typedef isf_status_t(* | fnStop_t )(void *apBusHandle, isf_duration_t aTimeout) |
| This is the function pointer signature for stopping the bus. More... | |
| typedef isf_status_t(* | fnConnectToEndpoint_t )(void *apBusHandle, void *apDevice, void **apEndpointHandle) |
| This is the function pointer signature for getting the Endpoint handle. More... | |
| typedef isf_status_t(* | fnDisconnectEndpoint_t )(void *apEndpointHandle) |
| This is the function pointer signature for closing the Endpoint. More... | |
| typedef isf_status_t(* | fnAcquireLock_t )(void *apBusHandle, isf_duration_t aTimeout) |
| This is the function pointer signature for acquiring the lock for a particular bus. More... | |
| typedef isf_status_t(* | fnReleaseLock_t )(void *apBusHandle) |
| This is the function pointer signature for releasing the lock for a particular bus. More... | |
| typedef isf_status_t(* | fnRead_t )(void *apEndpointHandle, int32 offset, void *apReadBuffer, uint32 buffsize, uint32 nBytesRead, comm_Flags_t aFlags) |
| This is the function pointer signature for reading the data from a specified device. More... | |
| typedef isf_status_t(* | fnWrite_t )(void *apEndpointHandle, int32 offset, uint8 *pWriteBuffer, uint32 buffsize, uint32 nBytesWrite, comm_Flags_t aFlags) |
| This is the the function pointer signature for writing the data to a specified device. More... | |
| typedef struct busHandle_struct | busHandle_t |
| This structure is a declaration of a BusHandle type. More... | |
isf_protocol_adapter.h defines the general interface definition for the protocol adapter.
File: isf_protocol_adapter.h
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file isf_protocol_adapter.h.
| typedef struct busHandle_struct busHandle_t |
This structure is a declaration of a BusHandle type.
| typedef isf_status_t(* fnAcquireLock_t)(void *apBusHandle, isf_duration_t aTimeout) |
This is the function pointer signature for acquiring the lock for a particular bus.
Definition at line 52 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnConfigure_t)(void *apBusHandle, void *apBusConfig) |
This is the function pointer signature for setting the configuration of the bus.
Definition at line 31 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnConnectToEndpoint_t)(void *apBusHandle, void *apDevice, void **apEndpointHandle) |
This is the function pointer signature for getting the Endpoint handle.
Definition at line 43 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnDisconnectEndpoint_t)(void *apEndpointHandle) |
This is the function pointer signature for closing the Endpoint.
Definition at line 47 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnGetConfig_t)(void *apBusHandle, void *apBusConfig) |
This is the function pointer signature for getting the configuration of the bus.
Definition at line 27 of file isf_protocol_adapter.h.
| typedef comm_State_t(* fnGetState_t)(void *apBusHandle) |
This is the function pointer signature for getting the state of the bus.
Definition at line 23 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnInit_t)(comm_Id_t aBusId, void *apBusHandle) |
This is the function pointer signature for bus initialization.
Definition at line 19 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnRead_t)(void *apEndpointHandle, int32 offset, void *apReadBuffer, uint32 buffsize, uint32 nBytesRead, comm_Flags_t aFlags) |
This is the function pointer signature for reading the data from a specified device.
Definition at line 60 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnReleaseLock_t)(void *apBusHandle) |
This is the function pointer signature for releasing the lock for a particular bus.
Definition at line 56 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnStart_t)(void *apBusHandle) |
This is the function pointer signature for starting the bus.
Definition at line 35 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnStop_t)(void *apBusHandle, isf_duration_t aTimeout) |
This is the function pointer signature for stopping the bus.
Definition at line 39 of file isf_protocol_adapter.h.
| typedef isf_status_t(* fnWrite_t)(void *apEndpointHandle, int32 offset, uint8 *pWriteBuffer, uint32 buffsize, uint32 nBytesWrite, comm_Flags_t aFlags) |
This is the the function pointer signature for writing the data to a specified device.
Definition at line 64 of file isf_protocol_adapter.h.