![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
isf_sensors.h contains the ISF Generic Sensor definitions and data structures required when a client task accesses accelerometer sensor data via the Sensor Manager API. More...


Go to the source code of this file.
Data Structures | |
| struct | DeviceDescriptor_struct |
| Define the sensor device descriptor. More... | |
Typedefs | |
| typedef struct DeviceDescriptor_struct | DeviceDescriptor_t |
| Define the sensor device descriptor. More... | |
Enumerations | |
| enum | sensor_mode_t { SENSOR_BOOT, SENSOR_STANDBY, SENSOR_READY, SENSOR_ACTIVE } |
| enum | { SENSOR_STATE_UNINITIALIZED, SENSOR_STATE_INITIALIZED, SENSOR_STATE_CONFIGURED, SENSOR_STATE_STARTED } |
| Define the sensor internal states. More... | |
| enum | { SENSOR_ERROR_CHECKID, SENSOR_ERROR_SETMODE, SENSOR_ERROR_GETDATA } |
| Define the sensor error status values. More... | |
isf_sensors.h contains the ISF Generic Sensor definitions and data structures required when a client task accesses accelerometer sensor data via the Sensor Manager API.
Definition in file isf_sensors.h.
| typedef struct DeviceDescriptor_struct DeviceDescriptor_t |
Define the sensor device descriptor.
| anonymous enum |
Define the sensor internal states.
| Enumerator | |
|---|---|
| SENSOR_STATE_UNINITIALIZED | |
| SENSOR_STATE_INITIALIZED | |
| SENSOR_STATE_CONFIGURED | |
| SENSOR_STATE_STARTED | |
Definition at line 30 of file isf_sensors.h.
| anonymous enum |
Define the sensor error status values.
| Enumerator | |
|---|---|
| SENSOR_ERROR_CHECKID | |
| SENSOR_ERROR_SETMODE | |
| SENSOR_ERROR_GETDATA | |
Definition at line 40 of file isf_sensors.h.
| enum sensor_mode_t |
| Enumerator | |
|---|---|
| SENSOR_BOOT | |
| SENSOR_STANDBY | |
| SENSOR_READY | |
| SENSOR_ACTIVE | |
Definition at line 19 of file isf_sensors.h.