![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The isf_sm_api.h contains the collection of APIs for the Sensor Manager as well as related defines and data structures required. More...


Go to the source code of this file.
Functions | |
| uint8 | isf_sm_find_sensor_by_type (isf_SensorTypes_t typeToFind, isf_SensorDataTypes_t dataTypeToFind, uint8 *sensorList, uint8 sensorListSize) |
| This is the Sensor Manager API used to find a sensor of the requested type. More... | |
| sm_result_t | isf_sm_subscribe_sensor_data (uint8 nSensorID, isf_SubscriptionSettings_t *pRequiredSettings, LWEVENT_STRUCT *pEventGroup, uint32 nEventFieldIndex, uint32 *pTokenAssigned) |
| This is the Sensor Manager API used to subscribe to sensor data. More... | |
| sm_result_t | isf_sm_unsubscribe_sensor_data (uint32 nTokenID) |
| This Sensor Manager API unsubscribes from receiving sensor data. More... | |
| sm_result_t | isf_sm_begin_sensor_data (uint32 nTokenID) |
| This Sensor Manager API allows a subscriber to receive sensor data. More... | |
| sm_result_t | isf_sm_end_sensor_data (uint32 nTokenID) |
| This Sensor Manager API is used by a subscriber to stop receiving sensor data. More... | |
| sm_result_t | isf_sm_get_sensor_data (uint32 nTokenID, void *pSensorData) |
| This Sensor Manager API allows a subscriber to fetch a new sensor data set. More... | |
The isf_sm_api.h contains the collection of APIs for the Sensor Manager as well as related defines and data structures required.
Definition in file isf_sm_api.h.
| sm_result_t isf_sm_begin_sensor_data | ( | uint32 | nTokenID | ) |
This Sensor Manager API allows a subscriber to receive sensor data.
This API allows a subscriber to request the Sensor Manager to begin sending subscribed sensor data.
| [in] | nTokenID | This is the tokenID received from the SM after subscribing to this sensor data. |
| ISF_SUCCESS | is returned when the current subscriber is capable to receive notifications when data is available from the indicated sensor. |
| SM_API_ERR_TOKEN_ID | is returned if the tokenID passed into the function is not valid. |
isf_sm_begin_sensor_data( hostAccelDataToken); Copyright (c) 2012, Freescale Semiconductor, Inc.
| sm_result_t isf_sm_end_sensor_data | ( | uint32 | nTokenID | ) |
This Sensor Manager API is used by a subscriber to stop receiving sensor data.
This API enables a subscriber to request the Sensor Manager to stop sending subscribed sensor data.
| [in] | nTokenID | The tokenID of the sensor from which the subscriber no longer wishes to receive data. |
| ISF_SUCCESS | is returned when the sensor no longer provides data to the subscriber. |
| SM_API_ERR_TOKEN_ID | is returned when the tokenID passed into the function is not valid. |
isf_sm_end_sensor_data( hostAccelDataToken);
Copyright (c) 2012, Freescale Semiconductor, Inc.
| uint8 isf_sm_find_sensor_by_type | ( | isf_SensorTypes_t | typeToFind, |
| isf_SensorDataTypes_t | dataTypeToFind, | ||
| uint8 * | sensorList, | ||
| uint8 | sensorListSize | ||
| ) |
This is the Sensor Manager API used to find a sensor of the requested type.
| [in] | typeToFind | The type of the sensor to search for. |
| [in] | dataTypeToFind | An additional data type that must be supported by the sensors. |
| [in,out] | sensorList | Pointer to a buffer for the returned sensor IDs |
| [in] | sensorListSize | The maximum number of sensorIDs to be returned (the size of the sensorList) |
| A | return value of zero indicates that no matching sensors were found. |
| A | non-zero return value indicates the number of sensorIDs that were placed in the sensorList that matched the specified search criteria. |
| sm_result_t isf_sm_get_sensor_data | ( | uint32 | nTokenID, |
| void * | pSensorData | ||
| ) |
This Sensor Manager API allows a subscriber to fetch a new sensor data set.
This API allows a subscriber to fetch the next data set(s) when notified of new data availability.
| [in] | nTokenID | The tokenID received from the SM when the subscriber subscribed to this sensor at the given rate. |
| [in,out] | pSensorData | On input,the parameter contains a valid pointer to the memory location to copy sensor sample set(s). On successful output, the parameter contains current sensor sample(s). When there is an error, the parameter is not changed. |
| ISF_SUCCESS | is returned upon the sensor data set is copied successfully to the proper location. |
| SM_API_ERR_TOKEN_ID | is returned when the tokenID passed into the function is not valid. |
The following outlines the sequence of actions occuring when a subscriber receives sensor data:
1. Subscriber waits for a specific event in its event group to receive sensor data from a given subscription.
2. The Sensor Manager signals the relevant event after depositing one or more new data sets in the shared memory area.
3. The subscriber, then, calls this API with the appropriate parameters as described above.
4. The API copies the sensor data set(s) to the passed in memory buffer with semaphore protection.
5. The subscriber task is free to use the sensor data as it pleases.
------------------------------------------------------------
Notes:
- When notified via an event, the subscriber is able to fetch the data with the API.
Or, the subscriber could decide not to get the data, at its discretion.
- The Sensor Manager over-writes the shared memory buffer set up during its subscription whenever new data is available based upon the sampling rate of this subscription.
- When an event notification is made by the Sensor Manager, the sensor data available to fetch is the most recent sample set(s).
Notes on the example code:
- gHostNoFifoAccelData : The user buffer for receiving accelerometer data when notified by the Sensor Manager that the accelerometer data is ready.
- EV_HOST_ACCEL_DATA_RDY : The event flag (bit) for the Sensor Manager to notify the user when new accelerometer data is available.
--------------------------------------------------------------
AccelData_t gHostNoFifoAccelData;
...
vuint8 *pv8MailBox;
uint8 *pSendData;
uint8 bytes2Write;
...
switch (gCurrentEventID)
{
case EV_HOST_ACCEL_DATA_RDY:
isf_sm_get_sensor_data(hostAccelDataToken, (void *)&gHostNoFifoAccelData );
// Now the data is consumed.
// This data is deposited in the Slave-Port Mailbox for the host application to fetch
// The accelerometer data packet starts writing from MB24.
// MB22 - MB25 : time stamp of this data set
// MB26 - MB31 : xyz data [6 bytes]
pv8MailBox = &SP_MB22;
pSendData = (uint8 *)&gHostNoFifoAccelData;
bytes2Write = (uint8)sizeof(gHostNoFifoAccelData);
while (bytes2Write--)
{
*pv8MailBox++ = *pSendData++;
}
break;
Copyright (c) 2012, Freescale Semiconductor, Inc.
| sm_result_t isf_sm_subscribe_sensor_data | ( | uint8 | nSensorID, |
| isf_SubscriptionSettings_t * | pRequiredSettings, | ||
| LWEVENT_STRUCT * | pEventGroup, | ||
| uint32 | nEventFieldIndex, | ||
| uint32 * | pTokenAssigned | ||
| ) |
This is the Sensor Manager API used to subscribe to sensor data.
| [in] | nSensorID | ISF unique sensor obtained from the sensor list. |
| [in,out] | pRequiredSettings | On input, the parameter contains a valid pointer to the desired sensor sample settings. On output, alternate sensor sample settings are provided, if the requested settings are not possible. |
| [in] | pEventGroup | Pointer to the event group for SM to signal when sensor data is ready. |
| [in] | nEventFieldIndex | Bit number or index in the event group for SM to signal when sensor data is ready. |
| [in,out] | pTokenAssigned | On input, parameter contains a valid pointer to memory to send the assigned token ID. On successful output, the parameter contains the assigned token ID. |
| ISF_SUCCESS | is returned when the subscriber is registered to receive sensor data for the given sampling settings. |
| SM_API_ALTERNATE_OFFERED | is returned when an alternate rate is provided. |
| SM_API_ERR_SENSOR_ID | is returned when an invalid sensor ID is provided. |
Otherwise, the subscriber is not registered to receive sensor data. Based on the return status, alternative sample settings may be proposed.
ACCEL_SENSOR_3D : The ID of the accelerometer sensor to subscribe to. Subscription_EventGrp : Event group for Sensor Manager to post events to this task when new accelerometer data is available. EV_ACCEL_DATA_RDY : event flag (bit) in the gHostProxy_EventGrp to be signaled. SM_GIVEN_SETTINGS : the sensor settings in the subscription must be used exactly. AccelDataToken : The unique returned token for the subscription.
SubscriptionSettings.nSamplePeriod = 20000; SubscriptionSettings.resultType = TYPE_RAW_ACCELERATION_3D; SubscriptionSettings.resultFormat = DSA_RESULT_TYPE_RAW_COUNTS; SubscriptionSettings.nFifoDepth = 1; SubscriptionSettings.nSettingsToUse = SM_GIVEN_SETTINGS;
smApiResult = isf_sm_subscribe_sensor_data( SM_AFE_ACCEL_SENSOR_3D,
&SubscriptionSettings,
&Subscription_EventGrp,
EV_ACCEL_DATA_RDY,
&AccelDataToken);
if ( smApiResult != ISF_SUCCESS)
{
// Error handling.
;
}
Copyright (c) 2014, Freescale Semiconductor, Inc.
*
| sm_result_t isf_sm_unsubscribe_sensor_data | ( | uint32 | nTokenID | ) |
This Sensor Manager API unsubscribes from receiving sensor data.
This API allow the subscriber to unregister from a previously registered subscription to sensor data.
| [in] | nTokenID | This is the tokenID received from the SM after subscribing to the sensor. |
| ISF_SUCCESS | is returned when the unsubscribe operation completes successfully. |
| SM_API_ERR_TOKEN_ID | is returned when the tokenID passed into the function is not valid. |
isf_sm_unsubscribe_sensor_data( hostAccelDataToken); Copyright (c) 2012, Freescale Semiconductor, Inc.