![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The isf_sm_types.h contains the collection of type definitions used in the Sensor Manager Interface as well as related defines and data structures required. More...


Go to the source code of this file.
Data Structures | |
| struct | isf_SubscriptionSettings_t |
Macros | |
| #define | SM_MAX_SUBSCRIBERS_PER_SENSOR (3) |
| This status code indicates that the API operation was successful. More... | |
| #define | SM_MAX_FIFO_DEPTH (20) |
| This is the maximum allowed depth of the sample FIFO. More... | |
| #define | SM_API_ERR_TOKEN_ID (sm_result_t)(-1L) |
| This is returned by the Sensor Manager when an invalid token ID is passed into any of the API calls. More... | |
| #define | SM_API_ERR_SENSOR_ID (sm_result_t)(-2L) |
| This is returned by the Sensor Manager when the passed parameter, sensor ID, does not match an existing sensor. More... | |
| #define | SM_API_ERR_ALREADY_BEGUN (sm_result_t)(-3L) |
| This is returned by the Sensor Manager when the sensor data flow is already enabled. More... | |
| #define | SM_API_ERR_NOT_YET_BEGUN (sm_result_t)(-4L) |
| This is returned by the Sensor Manager when the sensor data is unavailable because the data stream has not been started. More... | |
| #define | SM_API_ERR_SUBSCRIBER_COUNT (sm_result_t)(-5L) |
| This is returned by the Sensor Manager when the maximum number of subscribers as defined in SM_MAX_SUBSCRIBERS_PER_SENSOR for this particular sensor has been exceeded. More... | |
| #define | SM_API_ERR_NO_MEMORY (sm_result_t)(-6L) |
| This is returned by the Sensor Manager when an out-of- memory error status is returned during the execution of the API. More... | |
| #define | SM_API_ERR_FIFO_OVER_LIMIT (sm_result_t)(-7L) |
| This is returned by the Sensor Manager when the requested FIFO depth is larger than the FIFO limit specified in SM_MAX_FIFO_DEPTH. More... | |
| #define | SM_API_ERR_SAMPLE_TAP_RATE (sm_result_t)(-8L) |
| This is returned by the Sensor Manager when the requested sample tap rate is invalid. More... | |
| #define | SM_API_ERR_SETTINGS_TO_USE (sm_result_t)(-9L) |
| This is returned by the Sensor Manager when the requested sensor settings are invalid. More... | |
| #define | SM_API_ALTERNATE_OFFERED (sm_result_t)(-10L) |
| This is the status code returned by the Sensor Manager when the sensor cannot be configured based on user requested sensor settings. Additionally, the Sensor Manager provides a suggestion for the next best alternate rate and other possible settings. More... | |
| #define | SM_API_ERR_BUFFERLOCK_TIMEOUT (sm_result_t)(-11L) |
| This is returned by the Sensor Manager when the sample buffer lock call fails. More... | |
| #define | SM_API_ERR_LOCK_CREATION_FAILED (sm_result_t)(-12L) |
| This is returned by the Sensor Manager when the MQX semaphore create call fails. More... | |
| #define | SM_API_ERR_SENSOR_NOT_AVAIL (sm_result_t)(-21L) |
| This is returned by the Sensor Manager when the requested sensor is not available. More... | |
| #define | SM_API_ERR_SENSOR_ALREADY_INITIALIZED (sm_result_t)(-22L) |
| This is returned by the Sensor Manager when the sensor is already initialized. More... | |
| #define | SM_API_ERR_SENSOR_INIT_FAILED (sm_result_t)(-23L) |
| This is returned by the Sensor Manager when the sensor initialization was not successful. More... | |
| #define | SM_API_ERR_INVALID_HANDLE (sm_result_t)(-24L) |
| This is returned by the Sensor Manager when it receives an invalid handle. More... | |
| #define | SM_API_ERR_INVALID_PTR (sm_result_t)(-25L) |
| This is returned by the Sensor Manager when it receives an invalid pointer. More... | |
| #define | SM_API_ERR_MAX_TAPS_PER_SENSOR (sm_result_t)(-26L) |
| This is returned by the Sensor Manager when no more sensor taps are available. More... | |
| #define | SM_API_ERR_DATATYPE_NOT_SUPPORTED (sm_result_t)(-27L) |
| This is returned by the Sensor Manager when no more sensor taps are available. More... | |
Typedefs | |
| typedef int32 | sm_result_t |
| Sensor Manager API return type. More... | |
| typedef uint32 | sm_token_t |
| Sensor Manager subscription token type. More... | |
| typedef enum SubscriptionSettingChoices | SubscriptionSettingsChoices_t |
Enumerations | |
| enum | SubscriptionSettingChoices { SM_CURRENT_SETTINGS = 1, SM_GIVEN_SETTINGS, SM_BEST_POSSIBLE_SETTINGS } |
The isf_sm_types.h contains the collection of type definitions used in the Sensor Manager Interface as well as related defines and data structures required.
Definition in file isf_sm_types.h.
| #define SM_API_ALTERNATE_OFFERED (sm_result_t)(-10L) |
This is the status code returned by the Sensor Manager when the sensor cannot be configured based on user requested sensor settings. Additionally, the Sensor Manager provides a suggestion for the next best alternate rate and other possible settings.
Definition at line 116 of file isf_sm_types.h.
| #define SM_API_ERR_ALREADY_BEGUN (sm_result_t)(-3L) |
This is returned by the Sensor Manager when the sensor data flow is already enabled.
Definition at line 66 of file isf_sm_types.h.
| #define SM_API_ERR_BUFFERLOCK_TIMEOUT (sm_result_t)(-11L) |
This is returned by the Sensor Manager when the sample buffer lock call fails.
Definition at line 121 of file isf_sm_types.h.
| #define SM_API_ERR_DATATYPE_NOT_SUPPORTED (sm_result_t)(-27L) |
This is returned by the Sensor Manager when no more sensor taps are available.
Definition at line 164 of file isf_sm_types.h.
| #define SM_API_ERR_FIFO_OVER_LIMIT (sm_result_t)(-7L) |
This is returned by the Sensor Manager when the requested FIFO depth is larger than the FIFO limit specified in SM_MAX_FIFO_DEPTH.
Definition at line 95 of file isf_sm_types.h.
| #define SM_API_ERR_INVALID_HANDLE (sm_result_t)(-24L) |
This is returned by the Sensor Manager when it receives an invalid handle.
Definition at line 149 of file isf_sm_types.h.
| #define SM_API_ERR_INVALID_PTR (sm_result_t)(-25L) |
This is returned by the Sensor Manager when it receives an invalid pointer.
Definition at line 154 of file isf_sm_types.h.
| #define SM_API_ERR_LOCK_CREATION_FAILED (sm_result_t)(-12L) |
This is returned by the Sensor Manager when the MQX semaphore create call fails.
Definition at line 126 of file isf_sm_types.h.
| #define SM_API_ERR_MAX_TAPS_PER_SENSOR (sm_result_t)(-26L) |
This is returned by the Sensor Manager when no more sensor taps are available.
Definition at line 159 of file isf_sm_types.h.
| #define SM_API_ERR_NO_MEMORY (sm_result_t)(-6L) |
This is returned by the Sensor Manager when an out-of- memory error status is returned during the execution of the API.
Definition at line 88 of file isf_sm_types.h.
| #define SM_API_ERR_NOT_YET_BEGUN (sm_result_t)(-4L) |
This is returned by the Sensor Manager when the sensor data is unavailable because the data stream has not been started.
Definition at line 73 of file isf_sm_types.h.
| #define SM_API_ERR_SAMPLE_TAP_RATE (sm_result_t)(-8L) |
This is returned by the Sensor Manager when the requested sample tap rate is invalid.
Definition at line 101 of file isf_sm_types.h.
| #define SM_API_ERR_SENSOR_ALREADY_INITIALIZED (sm_result_t)(-22L) |
This is returned by the Sensor Manager when the sensor is already initialized.
Definition at line 139 of file isf_sm_types.h.
| #define SM_API_ERR_SENSOR_ID (sm_result_t)(-2L) |
This is returned by the Sensor Manager when the passed parameter, sensor ID, does not match an existing sensor.
Definition at line 61 of file isf_sm_types.h.
| #define SM_API_ERR_SENSOR_INIT_FAILED (sm_result_t)(-23L) |
This is returned by the Sensor Manager when the sensor initialization was not successful.
Definition at line 144 of file isf_sm_types.h.
| #define SM_API_ERR_SENSOR_NOT_AVAIL (sm_result_t)(-21L) |
This is returned by the Sensor Manager when the requested sensor is not available.
Definition at line 132 of file isf_sm_types.h.
| #define SM_API_ERR_SETTINGS_TO_USE (sm_result_t)(-9L) |
This is returned by the Sensor Manager when the requested sensor settings are invalid.
Definition at line 107 of file isf_sm_types.h.
| #define SM_API_ERR_SUBSCRIBER_COUNT (sm_result_t)(-5L) |
This is returned by the Sensor Manager when the maximum number of subscribers as defined in SM_MAX_SUBSCRIBERS_PER_SENSOR for this particular sensor has been exceeded.
Definition at line 81 of file isf_sm_types.h.
| #define SM_API_ERR_TOKEN_ID (sm_result_t)(-1L) |
This is returned by the Sensor Manager when an invalid token ID is passed into any of the API calls.
Definition at line 55 of file isf_sm_types.h.
| #define SM_MAX_FIFO_DEPTH (20) |
This is the maximum allowed depth of the sample FIFO.
Note: This define must not be changed by the user.
Definition at line 35 of file isf_sm_types.h.
| #define SM_MAX_SUBSCRIBERS_PER_SENSOR (3) |
This status code indicates that the API operation was successful.
This is the maximum number of subscribers allowed per sensor.
Note: This define must not be changed by the user.
Definition at line 28 of file isf_sm_types.h.
| typedef int32 sm_result_t |
Sensor Manager API return type.
Definition at line 38 of file isf_sm_types.h.
| typedef uint32 sm_token_t |
Sensor Manager subscription token type.
Definition at line 41 of file isf_sm_types.h.
| typedef enum SubscriptionSettingChoices SubscriptionSettingsChoices_t |
Defines for subscriber setting options.
Defines for subscriber setting options.
Definition at line 167 of file isf_sm_types.h.