![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
isf_spi_master_types.h defines the spi protocol adapter structure and types. More...


Go to the source code of this file.
Data Structures | |
| struct | spi_master_BusConfig_struct |
| struct | spi_mater_BusHandle_struct |
| This structure defines the data bus handle. More... | |
| struct | spi_mater_SlaveCmd |
| This structure defines the spi slave command format. More... | |
| struct | spi_mater_slaveInfo |
| This structure defines the slave specific spi information. More... | |
| struct | spi_master_CommSpecificInfo_t |
Typedefs | |
| typedef struct spi_master_BusConfig_struct | spi_master_busConfig_t |
| typedef struct spi_mater_BusHandle_struct | spi_master_busHandle_t |
| This structure defines the data bus handle. More... | |
| typedef struct spi_mater_SlaveCmd | spi_mater_slaveCmd_t |
| This structure defines the spi slave command format. More... | |
| typedef isf_status_t(* | fnslaveinit_t )(void) |
| typedef isf_status_t(* | fnwritepreProcessing_t )(void *cmdOut, uint32 offset, uint32 size, void *writebuffer) |
| typedef isf_status_t(* | fnwritepostProcossing_t )(void *cmd) |
| typedef isf_status_t(* | fnreadpreProcessing_t )(void *cmdout, uint32 offset, uint32 size) |
| typedef isf_status_t(* | fnreadpostProcossing_t )(void *cmd, void *dataOut) |
| typedef struct spi_mater_slaveInfo | spi_master_slaveInfo_t |
| This structure defines the slave specific spi information. More... | |
isf_spi_master_types.h defines the spi protocol adapter structure and types.
File: isf_spi_master_types.h
Copyright (c) 2014, Freescale Semiconductor, Inc.
Definition in file isf_spi_master_types.h.
| typedef isf_status_t(* fnreadpostProcossing_t)(void *cmd, void *dataOut) |
Definition at line 43 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnreadpreProcessing_t)(void *cmdout, uint32 offset, uint32 size) |
Definition at line 42 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnslaveinit_t)(void) |
Definition at line 39 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnwritepostProcossing_t)(void *cmd) |
Definition at line 41 of file isf_spi_master_types.h.
| typedef isf_status_t(* fnwritepreProcessing_t)(void *cmdOut, uint32 offset, uint32 size, void *writebuffer) |
Definition at line 40 of file isf_spi_master_types.h.
| typedef struct spi_master_BusConfig_struct spi_master_busConfig_t |
| typedef struct spi_mater_BusHandle_struct spi_master_busHandle_t |
This structure defines the data bus handle.
| typedef struct spi_mater_slaveInfo spi_master_slaveInfo_t |
This structure defines the slave specific spi information.
| typedef struct spi_mater_SlaveCmd spi_mater_slaveCmd_t |
This structure defines the spi slave command format.