![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
The isf_user_config.h file contains the user configurable settings to either include or exclude an ISF component. More...

Go to the source code of this file.
Macros | |
| #define | ISF_COMPONENT_CI (1) |
| When ISF_COMPONENT_SM is defined as 1, the Sensor Manager component is linked to the user application. More... | |
| #define | ISF_COMPONENT_BM (1) |
| When ISF_COMPONENT_BM is defined as 1, the Bus Mangement component code is compiled. Note: The component must be recompiled when this setting is changed. More... | |
| #define | ISF_COMPONENT_PM (1) |
| When defined as 1, the Power Management component code will compiled. The component must be recompiled when this setting is changed. More... | |
The isf_user_config.h file contains the user configurable settings to either include or exclude an ISF component.
Definition in file isf_user_config.h.
| #define ISF_COMPONENT_BM (1) |
When ISF_COMPONENT_BM is defined as 1, the Bus Mangement component code is compiled.
Note: The component must be recompiled when this setting is changed.
Definition at line 33 of file isf_user_config.h.
| #define ISF_COMPONENT_CI (1) |
When ISF_COMPONENT_SM is defined as 1, the Sensor Manager component is linked to the user application.
When ISF_COMPONENT_CI is defined as 1, the Command Interpreter component is linked to the user application.
Definition at line 22 of file isf_user_config.h.
| #define ISF_COMPONENT_PM (1) |
When defined as 1, the Power Management component
code will compiled. The component must be recompiled when this setting is changed.
Definition at line 44 of file isf_user_config.h.