![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Implements the ISF power management. More...
#include "isf_target.h"#include "isf.h"#include "lwevent.h"#include "lwsem.h"#include "mutex.h"#include "lwmem.h"#include "isf_bm.h"#include "isf_pm.h"#include "pm_internal.h"#include "cortex.h"#include "Cpu.h"
Go to the source code of this file.
Functions | |
| void | isr_pm_callback_sof (pointer dummy) |
| void | task_idle (uint32 initial_data) |
| isf_status_t | pm_init (void) |
| This API initializes the Power Manager. More... | |
| power_level_t | isf_power_set (power_level_t aLevel) |
| This API sets the requested power level for power management. More... | |
| power_level_t | isf_power_get (void) |
| This API returns the current power level for power management. More... | |
Variables | |
| volatile uint_32 | bsptimer_counter32 |
Implements the ISF power management.
Definition in file pm.c.
| power_level_t isf_power_get | ( | void | ) |
This API returns the current power level for power management.
The current power level setting of the Power Manager is returned.
| power_level_t isf_power_set | ( | power_level_t | aLevel | ) |
This API sets the requested power level for power management.
The Power Manager provides the capability to automatically control the power mode when the system is idle. Part of the power management is an idle task running at the lowest system priority. When all higher-priority tasks are blocked waiting for events, the idle task is executed. In the idle task, the system power state is set to one of the states described by the pm_power_level_enum values as specified as the argument to this API call.
The user may retrieves the current power level setting by invoking isf_power_get().
| [in] | aLevel | Power level of type power_level_t to set in the Power Manager. |
Definition at line 57 of file pm.c.
References ISF_POWER_LOW, ISF_POWER_NORMAL, and ISF_POWER_SLEEP.
Referenced by App1_ci_app_callback().

| void isr_pm_callback_sof | ( | pointer | dummy | ) |
| isf_status_t pm_init | ( | void | ) |
This API initializes the Power Manager.
The Power Manager requires a one-time initialization at system startup performed by this API call. It creates and initializes internal variables, and installs an interrupt service routine for the digital frame interrupt.
| ISF_SUCCESS | The initialization completes successfully. |
| ISF_ERR_LIB_INIT | Internal synchronization objects could not be created. |
Definition at line 44 of file pm.c.
References ISF_ERR_LIB_INIT, and ISF_SUCCESS.
Referenced by isf_lib_init().

| void task_idle | ( | uint32 | initial_data | ) |
Definition at line 156 of file pm.c.
References ISF_POWER_LOW, ISF_POWER_NORMAL, and ISF_POWER_SLEEP.
Referenced by PM_task().

| volatile uint_32 bsptimer_counter32 |