![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Power management header file. More...


Go to the source code of this file.
Macros | |
| #define | PM_DISABLE_INTERRUPTS() __disable_interrupt(); |
| #define | PM_ENABLE_INTERRUPTS() __enable_interrupt(); |
| #define | RTOSTIMER_STOP() { SYST_CSR &= ~SysTick_CSR_ENABLE_MASK; } |
| #define | RTOSTIMER_START() { SYST_CSR |= SysTick_CSR_ENABLE_MASK; } |
Power management header file.
Definition in file pm_internal.h.
| #define PM_DISABLE_INTERRUPTS | ( | ) | __disable_interrupt(); |
Definition at line 25 of file pm_internal.h.
| #define PM_ENABLE_INTERRUPTS | ( | ) | __enable_interrupt(); |
Definition at line 26 of file pm_internal.h.
| #define RTOSTIMER_START | ( | ) | { SYST_CSR |= SysTick_CSR_ENABLE_MASK; } |
Definition at line 32 of file pm_internal.h.
| #define RTOSTIMER_STOP | ( | ) | { SYST_CSR &= ~SysTick_CSR_ENABLE_MASK; } |
Definition at line 30 of file pm_internal.h.