![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure contains Timer Unit LLD function pointers. More...
#include <isf_fsl_TU_PEx.h>

This structure contains Timer Unit LLD function pointers.
Definition at line 55 of file isf_fsl_TU_PEx.h.
| fnTUDeinit_t fnTULDDDeint |
De-initialize a Timer Unit LDD component.
Definition at line 57 of file isf_fsl_TU_PEx.h.
| fnTUDisable_t fnTULDDDisable |
Disable a Timer Unit LDD component.
Definition at line 59 of file isf_fsl_TU_PEx.h.
Referenced by pit_hal_timer_stop().
| fnTUEnable_t fnTULDDEnable |
Enable a Timer Unit LDD component.
Definition at line 58 of file isf_fsl_TU_PEx.h.
Referenced by pit_hal_timer_start().
| fnTUGetCounterValue_t fnTULDDGetCounter |
Get the current value of the Timer Unit counter.
Definition at line 63 of file isf_fsl_TU_PEx.h.
Referenced by pit_hal_read_timer_count().
| fnTUGetPeriodTicks_t fnTULDDGetPeriod |
Get the Timer Unit period.
Definition at line 61 of file isf_fsl_TU_PEx.h.
Referenced by pit_hal_read_timer_count(), and pit_hal_read_timer_period_count().
| fnTUInit_t fnTULDDInit |
Initialize a Timer Unit LDD component.
Definition at line 56 of file isf_fsl_TU_PEx.h.
Referenced by pit_init_channel().
| fnTUResetCounter_t fnTULDDResetCounter |
Reset the Timer Unit counter.
Definition at line 62 of file isf_fsl_TU_PEx.h.
Referenced by pit_hal_timer_reset().
| fnTUSetPeriodTicks_t fnTULDDSetPeriod |
Set a Timer Unit period.
Definition at line 60 of file isf_fsl_TU_PEx.h.
Referenced by pit_hal_set_timer_period_count().