![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
Runtime state of the UART driver. More...
#include <fsl_uart_driver.h>

Data Fields | |
| uint32_t | instance |
| LDD_TDeviceData * | pDeviceHandle |
| LWEVENT_STRUCT | uartEventHandler |
Runtime state of the UART driver.
This struct holds data that are used by the UART peripheral driver to communicate between the transfer function and the interrupt handler. The interrupt handler also uses this information to keep track of its progress. The user is only responsible to pass in the memory for this run-time state structure where the UART driver will take care of filling out the members.
Definition at line 40 of file fsl_uart_driver.h.
| uint32_t instance |
UART module instance number.
Definition at line 41 of file fsl_uart_driver.h.
Referenced by uart_adapter_configure(), uart_adapter_start(), uart_adapter_stop(), uart_init(), uart_receive_data(), uart_receive_data_async(), uart_send_data(), and uart_send_data_async().
| LDD_TDeviceData* pDeviceHandle |
Pointer to the device handle.
Definition at line 42 of file fsl_uart_driver.h.
Referenced by uart_init(), uart_receive_data(), and uart_send_data().
| LWEVENT_STRUCT uartEventHandler |
Definition at line 43 of file fsl_uart_driver.h.
Referenced by Serial_ISF_UART1_OnBlockReceived(), Serial_ISF_UART1_OnBlockSent(), uart_init(), uart_receive_data(), and uart_send_data().