![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure holds information to receive a packet of data to the host. CI will fill the structure with the information as it receives it from the ISR and will notify the CI task when a packet has been fully received. More...
#include <task_ci.h>

Data Fields | |
| volatile ci_recv_state_t | rxState |
| volatile uint8 | mbIndex |
| Internal receive state. More... | |
| volatile uint8 | packetSize |
| Mailbox index. More... | |
| volatile uint8 * | pRxbuf |
| Expected packet size. More... | |
This structure holds information to receive a packet of data to the host. CI will fill the structure with the information as it receives it from the ISR and will notify the CI task when a packet has been fully received.
| volatile uint8 mbIndex |
Internal receive state.
Definition at line 78 of file task_ci.h.
Referenced by process_recv_byte(), and task_ci().
| volatile uint8 packetSize |
| volatile uint8* pRxbuf |
Expected packet size.
Definition at line 80 of file task_ci.h.
Referenced by ci_init(), process_recv_byte(), and task_ci().
| volatile ci_recv_state_t rxState |
Definition at line 77 of file task_ci.h.
Referenced by process_recv_byte().