![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation. More...
#include <fsl_fxas21002_i2cspi_3D_gyro.h>

Data Fields | |
| uint32 | periodNormalMode |
| uint8 | configVal |
the structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation.
Definition at line 82 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| uint8 configVal |
configuration value correspond to given ODR in millisecond.
Definition at line 84 of file fsl_fxas21002_i2cspi_3D_gyro.h.
| uint32 periodNormalMode |
Normal Mode ODR value in millisecond.
Definition at line 83 of file fsl_fxas21002_i2cspi_3D_gyro.h.