![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <fxas21002.h>

Data Fields | |
| uint8 | bandwidth |
| uint8 | gyroFullScaleRange |
| uint8 | wraptoone |
| uint8 | extctrlen |
| uint8 | fsdouble |
| uint32 | regCount |
| fxas21002_Sensor_Specific_Reg_t | regPairs [] |
Definition at line 213 of file fxas21002.h.
| uint8 bandwidth |
Definition at line 215 of file fxas21002.h.
| uint8 extctrlen |
Definition at line 218 of file fxas21002.h.
| uint8 fsdouble |
Definition at line 219 of file fxas21002.h.
| uint8 gyroFullScaleRange |
Definition at line 216 of file fxas21002.h.
| uint32 regCount |
Definition at line 220 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure().
| fxas21002_Sensor_Specific_Reg_t regPairs[] |
Definition at line 221 of file fxas21002.h.
Referenced by fsl_fxas21002_i2cspi_3D_gyro_Configure().
| uint8 wraptoone |
Definition at line 217 of file fxas21002.h.