![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
the structure defines the configuration table. More...
#include <fsl_fxos8700_i2cspi_6D_AccMag.h>

Data Fields | |
| void * | memberVariable |
| uint8 | startAddress |
| uint8 | size |
the structure defines the configuration table.
Definition at line 102 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| void* memberVariable |
reference to the member variable.
Definition at line 103 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| uint8 size |
size of the memeber to be configured.
Definition at line 105 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| uint8 startAddress |
start address to the member variable.
Definition at line 104 of file fsl_fxos8700_i2cspi_6D_AccMag.h.