![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_fxos8700_i2cspi_6D_AccMag.h>

Data Fields | |
| uint32 | timeStamp |
| int16 | accel [3] |
| int16 | mag [3] |
| uint8 | addr |
This structure defines the dummy DSA data buffer format.
Definition at line 109 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
| int16 accel[3] |
The accelerometer data
Definition at line 111 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
Referenced by fsl_fxos8700_i2cspi_6D_AccMag_Initialize(), and fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback().
| uint8 addr |
The device "address" can uniquely identify the sensor
Definition at line 113 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
Referenced by fsl_fxos8700_i2cspi_6D_AccMag_Initialize().
| int16 mag[3] |
The magnetometer data
Definition at line 112 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
Referenced by fsl_fxos8700_i2cspi_6D_AccMag_Initialize(), and fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback().
| uint32 timeStamp |
The time stamp for the data packet.
Definition at line 110 of file fsl_fxos8700_i2cspi_6D_AccMag.h.
Referenced by fsl_fxos8700_i2cspi_6D_AccMag_Initialize(), and fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback().