![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <isf_dsa_direct_types.h>

Data Fields | |
| isf_SensorDataTypes_t | resultType |
| The desired data type of the subscription. More... | |
| isf_dsa_result_types_t | resultFormat |
| The format of the data to be returned- 0=RAW, 1=FIXED, 2=FLOAT. More... | |
| uint32 | nSamplePeriod |
| Sample period in microseconds. More... | |
| uint8 | nSettingsToUse |
| 1 = current; 2=given; 3=best possible More... | |
| uint8 | nFifoDepth |
| 1 = no FIFO, or another value < SM_MAX_FIFO_DEPTH More... | |
Sensor configuration settings used when subscribing to sensor data.
Definition at line 23 of file isf_dsa_direct_types.h.
| uint8 nFifoDepth |
1 = no FIFO, or another value < SM_MAX_FIFO_DEPTH
Definition at line 29 of file isf_dsa_direct_types.h.
Referenced by App1_MainTask(), and fsl_fusion_virt_3D_orient_Configure().
| uint32 nSamplePeriod |
Sample period in microseconds.
Definition at line 27 of file isf_dsa_direct_types.h.
Referenced by App1_ci_app_callback(), App1_MainTask(), configure_sensor(), and fsl_fusion_virt_3D_orient_Configure().
| uint8 nSettingsToUse |
1 = current; 2=given; 3=best possible
Definition at line 28 of file isf_dsa_direct_types.h.
Referenced by App1_MainTask(), and fsl_fusion_virt_3D_orient_Configure().
| isf_dsa_result_types_t resultFormat |
The format of the data to be returned- 0=RAW, 1=FIXED, 2=FLOAT.
Definition at line 26 of file isf_dsa_direct_types.h.
Referenced by App1_MainTask(), configure_sensor(), and fsl_fusion_virt_3D_orient_Configure().
| isf_SensorDataTypes_t resultType |
The desired data type of the subscription.
Definition at line 25 of file isf_dsa_direct_types.h.
Referenced by App1_MainTask(), configure_sensor(), and fsl_fusion_virt_3D_orient_Configure().