![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This defines the DSA adapter functional interface. More...
#include <isf_dsa_adapter.h>

Data Fields | |
| LWEVENT_STRUCT * | pEventGroup |
| uint32 | nEventFieldIndex |
| isf_dsa_SensorSettings_t | sensorSettings |
This defines the DSA adapter functional interface.
Definition at line 92 of file isf_dsa_adapter.h.
| uint32 nEventFieldIndex |
The event flag of the event group to signal after depositing sensor sample in pSampleBuffer.
Definition at line 95 of file isf_dsa_adapter.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_PeriodicCallback(), and init_sensor().
| LWEVENT_STRUCT* pEventGroup |
The event group to signal after depositing sensor sample in pDataBuff.
Definition at line 94 of file isf_dsa_adapter.h.
Referenced by fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_PeriodicCallback(), and init_sensor().
| isf_dsa_SensorSettings_t sensorSettings |
The configuration parameters from the user including the fifo to use
Definition at line 96 of file isf_dsa_adapter.h.
Referenced by configure_sensor(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_Configure(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_Configure(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_Configure(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma865x_i2c_3D_accel_Configure(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mpl3115_i2c_1D_press_Configure(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().