![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This defines the DSA adapter device information block. More...
#include <isf_dsa_adapter.h>

Data Fields | |
| isf_SensorTypes_t * | pSupportedSensorTypes |
| isf_SensorDataTypes_t * | pSupportedSensorDataTypes |
| uint8 | nNativeDataSetSize |
This defines the DSA adapter device information block.
Definition at line 70 of file isf_dsa_adapter.h.
| uint8 nNativeDataSetSize |
The size of the native data set for this sensor.
Definition at line 74 of file isf_dsa_adapter.h.
Referenced by fsl_fusion_virt_3D_orient_Configure(), and isf_dsa_get_sizeof_native_data_type().
| isf_SensorDataTypes_t* pSupportedSensorDataTypes |
Pointer to a zero-terminated array of sensor data types
Definition at line 73 of file isf_dsa_adapter.h.
Referenced by isf_dsa_get_sensor_data_types().
| isf_SensorTypes_t* pSupportedSensorTypes |
Pointer to a zero-terminated array of sensor types
Definition at line 72 of file isf_dsa_adapter.h.
Referenced by isf_dsa_get_sensor_types().