![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_mpl3115_i2c_1D_press.h>

Data Fields | |
| uint32 | timestamp |
| Time stamp value in micro-seconds. More... | |
| uint32 | pressure |
| int32 | altitude |
| int16 | temperature |
This structure defines the dummy DSA data buffer format.
Definition at line 52 of file fsl_mpl3115_i2c_1D_press.h.
| int32 altitude |
Sensor altitude output: 2's complement 20-bits justified to MSBs; MS 16-bits are integer meters; LS 4-bits are fractional meters.
Definition at line 59 of file fsl_mpl3115_i2c_1D_press.h.
Referenced by fsl_mpl3115_i2c_1D_press_Initialize(), and mpl3115_GetData().
| uint32 pressure |
Sensor pressure output: unsigned 20-bits justified to MSBs; MS 18-bits are integer Pascals; LS 2-bits are fractional Pascals.
Definition at line 56 of file fsl_mpl3115_i2c_1D_press.h.
Referenced by fsl_mpl3115_i2c_1D_press_Initialize(), and mpl3115_GetData().
| int16 temperature |
Sensor temperature output; 2's complement 12-bits justified to MSBs; MS 8-bits are integer degrees Celsius; LS 4-bits are fractional degrees Celsius.
Definition at line 62 of file fsl_mpl3115_i2c_1D_press.h.
Referenced by fsl_mpl3115_i2c_1D_press_Initialize(), and mpl3115_GetData().
| uint32 timestamp |
Time stamp value in micro-seconds.
Definition at line 54 of file fsl_mpl3115_i2c_1D_press.h.
Referenced by fsl_mpl3115_i2c_1D_press_Initialize(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().