![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines important settings. More...
#include <fsl_mpl3115_i2c_1D_press.h>

Data Fields | |
| uint8 | sampleRateIndex |
| Holds the ODR index into the rate array fsl_mpl3115_period */. More... | |
This structure defines important settings.
Definition at line 46 of file fsl_mpl3115_i2c_1D_press.h.
| uint8 sampleRateIndex |
Holds the ODR index into the rate array fsl_mpl3115_period */.
Definition at line 48 of file fsl_mpl3115_i2c_1D_press.h.