![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "App1_Functions.h"#include "App1.h"#include "App1_types.h"#include "isf_target.h"#include "isf_types.h"#include "isf.h"#include "isf_init.h"#include "isf_ci.h"#include "isf_ci_stream.h"#include "isf_sm_types.h"#include "fsl_os_abstraction.h"#include "isf_util.h"#include "isf_dsa_direct.h"#include "isf_pm.h"#include "Events.h"#include "isf_sensor_configuration.h"#include "isf_sensor_configuration_extern.h"#include "isf_accelerometer_types.h"#include "isf_magnetometer_types.h"#include "isf_gyrometer_types.h"#include "isf_pressure_types.h"#include "isf_temperature_types.h"#include "isf_orientation_types.h"#include "isf_altitude_types.h"#include "isf_pedometer_types.h"#include "fsl_Sensor_Custom_1_Functions.h"#include "fsl_Sensor_Analog_1_Functions.h"
Go to the source code of this file.
Data Structures | |
| struct | subscriptionConfig_t |
| This structure holds the sensor subscriptions configuration info. More... | |
| struct | pseudoSettings_t |
| struct | appSubscriptionResponse_t |
| This structure holds the ISF application subscriptions information in the "GET_APP_SUBSCRIPTION" CI command response buffer. More... | |
Macros | |
| #define | App1_TASK_NAME "App1_task" |
| #define | App1_TASK_STACK_SIZE 1200 |
| #define | App1_TASK_PRIORITY 11 |
| #define | startof(type, member) ((int32)&((type *)0)->member) |
| #define | NUM_SENSORS (sizeof(App1AppInstance.info)/sizeof(SensorInfo_t)) |
| Macro thats holds number of active sensors. More... | |
| #define | SET_FIELD(name, val) (((val)<<name##_SHIFT)&(name##_MASK)) |
| Macro that extracts one of the fields below. More... | |
| #define | GET_FIELD(name, val) ((val&name##_MASK)>>name##_SHIFT) |
| #define | CTRL_STATE_MASK 0x0F |
| Control register mask/shift definitions for the application. More... | |
| #define | CTRL_STATE_SHIFT 0 |
| #define | CTRL_QREN_MASK 0x10 |
| #define | CTRL_QREN_SHIFT 4 |
| #define | CTRL_RESET_MASK 0x20 |
| #define | CTRL_RESET_SHIFT 5 |
| #define | CTRL_POWER_MASK 0xC0 |
| #define | CTRL_POWER_SHIFT 6 |
Functions | |
| OSA_TASK_DEFINE (App1, App1_TASK_STACK_SIZE) | |
| int32 | App1_GotoState (uint8 desiredState) |
| void | App1_task (os_task_param_t task_init_data) |
| void | App1_init (void) |
| void | App1_MainTask (void) |
| ci_response_t | App1_ci_app_callback (ci_host_cmd_packet_t *pHostPacket, ci_app_resp_packet_t *pAppPacket) |
| void | App1_ReturnSensorsToInit () |
Variables | |
| App1AppInstance_t | App1AppInstance |
Definition in file App1.c.