![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "isf_dsa_adapter.h"#include "isf_accelerometer_types.h"#include "isf.h"#include "isf_magnetometer_types.h"#include "isf_gyrometer_types.h"#include "isf_pressure_types.h"#include "isf_temperature_types.h"#include "isf_orientation_types.h"#include "isf_altitude_types.h"#include "isf_pedometer_types.h"#include "fsl_Sensor_Custom_1_Functions.h"#include "isf_sm_types.h"#include "fsl_Sensor_Analog_1_Functions.h"

Go to the source code of this file.
Data Structures | |
| struct | App1_app_info_t |
| struct | App1SensorData_t |
| struct | SensorInfo_t |
| struct | App1AppSettings_t |
| struct | App1AppInstance_t |
Enumerations | |
| enum | App1AppState_t { App1_STATE_STOPPED_UNSUBSCRIBED = 0, App1_STATE_STOPPED_SUBSCRIBED, App1_STATE_STARTED_SUBSCRIBED } |
| #define App1_Accelerometer0_DATA_READY_EVENT ((uint32)(1 << 0)) |
Definition at line 117 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer1_DATA_READY_EVENT ((uint32)(1 << 1)) |
Definition at line 119 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer2_DATA_READY_EVENT ((uint32)(1 << 2)) |
Definition at line 121 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer3_DATA_READY_EVENT ((uint32)(1 << 3)) |
Definition at line 123 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer4_DATA_READY_EVENT ((uint32)(1 << 4)) |
Definition at line 125 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer5_DATA_READY_EVENT ((uint32)(1 << 5)) |
Definition at line 127 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer6_DATA_READY_EVENT ((uint32)(1 << 6)) |
Definition at line 129 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Accelerometer7_DATA_READY_EVENT ((uint32)(1 << 7)) |
Definition at line 131 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_ALL_SENSOR_DATA_READY (1048575) |
Definition at line 157 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Altitude15_DATA_READY_EVENT ((uint32)(1 << 15)) |
Definition at line 147 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Analog19_DATA_READY_EVENT ((uint32)(1 << 19)) |
Definition at line 155 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_APP_DATA "" |
Definition at line 9 of file App1_types.h.
| #define App1_Custom18_DATA_READY_EVENT ((uint32)(1 << 18)) |
Definition at line 153 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Gyrometer10_DATA_READY_EVENT ((uint32)(1 << 10)) |
Definition at line 137 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Gyrometer11_DATA_READY_EVENT ((uint32)(1 << 11)) |
Definition at line 139 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Magnetometer8_DATA_READY_EVENT ((uint32)(1 << 8)) |
Definition at line 133 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Magnetometer9_DATA_READY_EVENT ((uint32)(1 << 9)) |
Definition at line 135 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Orientation14_DATA_READY_EVENT ((uint32)(1 << 14)) |
Definition at line 145 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Pedometer16_DATA_READY_EVENT ((uint32)(1 << 16)) |
Definition at line 149 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Pedometer17_DATA_READY_EVENT ((uint32)(1 << 17)) |
Definition at line 151 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Pressure12_DATA_READY_EVENT ((uint32)(1 << 12)) |
Definition at line 141 of file App1_types.h.
Referenced by App1_MainTask().
| #define App1_Temperature13_DATA_READY_EVENT ((uint32)(1 << 13)) |
Definition at line 143 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB0 1 |
Definition at line 74 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB1 1 |
Definition at line 76 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB10 1 |
Definition at line 94 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB11 1 |
Definition at line 96 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB12 1 |
Definition at line 98 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB13 1 |
Definition at line 100 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB14 1 |
Definition at line 102 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB15 1 |
Definition at line 104 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB16 1 |
Definition at line 106 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB17 1 |
Definition at line 108 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB18 1 |
Definition at line 110 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB19 1 |
Definition at line 112 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB2 1 |
Definition at line 78 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB3 1 |
Definition at line 80 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB4 1 |
Definition at line 82 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB5 1 |
Definition at line 84 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB6 1 |
Definition at line 86 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB7 1 |
Definition at line 88 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB8 1 |
Definition at line 90 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_FIFO_LEN_SUB9 1 |
Definition at line 92 of file App1_types.h.
Referenced by App1_MainTask().
| #define DATA_TYPE_SUB0 FXLC95000_1_DATA_TYPE |
Definition at line 75 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB1 FXLC95000_2_DATA_TYPE |
Definition at line 77 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB10 FXAS21002_1_DATA_TYPE |
Definition at line 95 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB11 FXAS21002_2_DATA_TYPE |
Definition at line 97 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB12 MPL3115_1_DATA_TYPE |
Definition at line 99 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB13 MPL3115_1_DATA_TYPE |
Definition at line 101 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB14 ORIENT_1_DATA_TYPE |
Definition at line 103 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB15 MPL3115_1_DATA_TYPE |
Definition at line 105 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB16 MMA955x_1_DATA_TYPE |
Definition at line 107 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB17 MMA955x_2_DATA_TYPE |
Definition at line 109 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB18 Custom_1_DATA_TYPE |
Definition at line 111 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB19 Analog_1_DATA_TYPE |
Definition at line 113 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB2 FXLS8471_1_DATA_TYPE |
Definition at line 79 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB3 FXLS8471_2_DATA_TYPE |
Definition at line 81 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB4 FXLS8952_1_DATA_TYPE |
Definition at line 83 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB5 FXOS8700_1_DATA_TYPE |
Definition at line 85 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB6 MMA8491Q_1_DATA_TYPE |
Definition at line 87 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB7 MMA865x_1_DATA_TYPE |
Definition at line 89 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB8 FXOS8700_2_DATA_TYPE |
Definition at line 91 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| #define DATA_TYPE_SUB9 MAG3110_1_DATA_TYPE |
Definition at line 93 of file App1_types.h.
Referenced by App1_MainTask(), and BasicApp1_OnAnySensor_Data_Ready().
| enum App1AppState_t |
| Enumerator | |
|---|---|
| App1_STATE_STOPPED_UNSUBSCRIBED | |
| App1_STATE_STOPPED_SUBSCRIBED | |
| App1_STATE_STARTED_SUBSCRIBED | |
Definition at line 185 of file App1_types.h.