![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
header for current pit instance. More...
#include "BMTIMER1.h"

Go to the source code of this file.
Macros | |
| #define | ISF_BM_PIT_INSTANCE FSL_BMTIMER1 |
| #define | ISF_BM_PIT_CHANNEL_NO FSL_BMTIMER1_CHANNEL |
| #define | ISF_BM_PIT_INSTANCER (clockMan1_InitConfig4) |
| #define | BM_PIT_SCALER (24) |
| #define | BM_PIT_SOURCE_CLK (24000000) |
| #define | BM_ROLLOVER_PERIOD (0x100000000/BM_PIT_SCALER) |
header for current pit instance.
Definition in file BM_pit_instance.h.
| #define BM_PIT_SCALER (24) |
Definition at line 19 of file BM_pit_instance.h.
| #define BM_PIT_SOURCE_CLK (24000000) |
Definition at line 20 of file BM_pit_instance.h.
| #define BM_ROLLOVER_PERIOD (0x100000000/BM_PIT_SCALER) |
Definition at line 21 of file BM_pit_instance.h.
| #define ISF_BM_PIT_CHANNEL_NO FSL_BMTIMER1_CHANNEL |
Definition at line 17 of file BM_pit_instance.h.
Referenced by bm_powerdown(), bm_start(), isr_bm_callback_tmr(), and Timer_IRQHandler().
| #define ISF_BM_PIT_INSTANCE FSL_BMTIMER1 |
Definition at line 16 of file BM_pit_instance.h.
Referenced by bm_powerdown(), bm_start(), isr_bm_callback_tmr(), and Timer_IRQHandler().
| #define ISF_BM_PIT_INSTANCER (clockMan1_InitConfig4) |
Definition at line 18 of file BM_pit_instance.h.