![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "BasicApp1_Functions.h"#include "BasicApp1.h"#include "BasicApp1_types.h"#include "isf_dsa_direct.h"#include "isf_sensor_configuration.h"#include "isf_sensor_configuration_extern.h"#include "isf_ci_stream.h"#include "isf_accelerometer_types.h"#include "isf_magnetometer_types.h"#include "isf_gyrometer_types.h"#include "isf_pressure_types.h"#include "isf_temperature_types.h"#include "isf_orientation_types.h"#include "isf_altitude_types.h"#include "isf_pedometer_types.h"#include "fsl_Sensor_Custom_1_Functions.h"#include "fsl_Sensor_Analog_1_Functions.h"
Go to the source code of this file.
Macros | |
| #define | BasicApp1_TASK_NAME "BasicApp1_task" |
| #define | BasicApp1_TASK_STACK_SIZE 1200 |
| #define | BasicApp1_TASK_PRIORITY 11 |
Functions | |
| OSA_TASK_DEFINE (BasicApp1, BasicApp1_TASK_STACK_SIZE) | |
| ci_response_t | BasicApp1_ci_app_callback (ci_host_cmd_packet_t *pHostPacket, ci_app_resp_packet_t *pAppPacket) |
| void | BasicApp1_MainTask (os_task_param_t task_init_data) |
| void | BasicApp1_init (void) |
| int8 | BasicApp1_FlashSensor (uint8 numBytes, uint8 *pFlashData) |
Definition in file BasicApp1.c.