![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This is user's event module. Put your event handler code here. More...
#include "Cpu.h"#include "Events.h"#include "rtos_main_task.h"#include "os_tasks.h"#include "App1_Functions.h"#include "BasicApp1_Functions.h"#include "fsl_Sensor_Custom_1_Functions.h"#include "fsl_Sensor_Analog_1_Functions.h"#include "BasicApp1_types.h"
Go to the source code of this file.
Functions | |
| void | BasicApp1_Initialization () |
| void | BasicApp1_CI_Callback (void *p_HostPacket, void *p_AppPacket, uint8_t *response) |
| void | BasicApp1_OnAnySensor_Data_Ready (uint8_t sensorIdx, uint32_t signalledEvents, void **pAppSensorData, void *pAppDataBuffers) |
This is user's event module. Put your event handler code here.
Definition in file BasicApp1_Functions.c.