![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "fsl_device_registers.h"#include "fsl_clock_manager.h"#include "fsl_mcg_hal.h"#include "fsl_sim_hal.h"#include "fsl_osc_hal.h"#include "fsl_rtc_hal.h"#include "fsl_port_hal.h"#include "fsl_interrupt_manager.h"#include "fsl_uart_hal.h"#include "fsl_uart_driver.h"#include "fsl_mpu_hal.h"#include "fsl_mpu_driver.h"#include "fsl_hwtimer.h"#include "fsl_os_abstraction.h"#include "osa1.h"#include "fsl_i2c_hal.h"#include "fsl_i2c_master_driver.h"#include "fsl_i2c_slave_driver.h"#include "fsl_i2c_shared_function.h"#include "fsl_dspi_hal.h"#include "fsl_dspi_master_driver.h"#include "fsl_dspi_slave_driver.h"#include "fsl_dspi_shared_function.h"#include "fsl_gpio_hal.h"#include "fsl_gpio_driver.h"#include "fsl_adc16_hal.h"#include "fsl_adc16_driver.h"#include "fsl_pit_hal.h"#include "fsl_pit_driver.h"#include <assert.h>
Go to the source code of this file.
Macros | |
| #define | CPU_PERIPHERALS_INIT 0x00U /* Peripherals_Init() method is not called in PE_low_level_init() */ |
| #define | CPU_COMPONENTS_INIT 0x01U /* Call Components_Init() method in PE_low_level_init() */ |
| #define | CPU_INIT_CONFIG 0x00U /* Do not include Init_Config.h in the main.c file */ |
| #define | CPU_HARDWARE_INIT 0x01U /* Call hardware_init() method in PE_low_level_init() */ |
Functions | |
| void | Components_Init (void) |
| void | PE_low_level_init (void) |
Definition in file Cpu.h.