![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "ISF_UART1.h"
Go to the source code of this file.
Functions | |
| void | UART_DRV_IRQHandler (uint32_t instance) |
| void | ISF_UART1_IRQHandler (void) |
Variables | |
| const uart_user_config_t | ISF_UART1_InitConfig0 |
| UART configuration declaration. More... | |
| uart_state_t | ISF_UART1_State |
Definition in file ISF_UART1.c.